<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC2387 interface with MM74HC573 -  3 state problem in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2387-interface-with-MM74HC573-3-state-problem/m-p/551051#M14121</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Erez on Thu Sep 24 02:18:16 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Im using P1[17] as out_control for MM74HC573.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When i first connect the voltage or reset the system, i am getting voltage 2[v] ( ONly voltage above 3[v] means '1')&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This is a big problem. i need the value to be '1' (or '0').&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;How can i solves this?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I've tried some actions:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Disabled the P1[17]&amp;nbsp; ENET-MDIO option&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Tried to write directly to the register- no effect &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Tried to connect pull up resistor.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Could someone help in this please?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;By the way,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have already a system that works perfect when i use the P0[26] for outcontrol.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:50:50 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:50:50Z</dc:date>
    <item>
      <title>LPC2387 interface with MM74HC573 -  3 state problem</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2387-interface-with-MM74HC573-3-state-problem/m-p/551051#M14121</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Erez on Thu Sep 24 02:18:16 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Im using P1[17] as out_control for MM74HC573.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When i first connect the voltage or reset the system, i am getting voltage 2[v] ( ONly voltage above 3[v] means '1')&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This is a big problem. i need the value to be '1' (or '0').&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;How can i solves this?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I've tried some actions:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Disabled the P1[17]&amp;nbsp; ENET-MDIO option&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Tried to write directly to the register- no effect &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Tried to connect pull up resistor.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Could someone help in this please?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;By the way,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have already a system that works perfect when i use the P0[26] for outcontrol.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:50:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2387-interface-with-MM74HC573-3-state-problem/m-p/551051#M14121</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:50:50Z</dc:date>
    </item>
  </channel>
</rss>