<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC2919 not able to program anymore</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2919-not-able-to-program-anymore/m-p/550815#M14082</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by deSteini on Wed Jun 04 01:31:04 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I figured out that i am able to flash the Board with Keil, but not use the DebuggerMode in Keil. After the Flash, the Power LED works normal and the Code almost, too. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;But if i am going then back to the IAR Workbench and try to flash/debugg, i get the same problem as before, connection Problems and LED goes out...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Somebody has a hint?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:50:46 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:50:46Z</dc:date>
    <item>
      <title>LPC2919 not able to program anymore</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2919-not-able-to-program-anymore/m-p/550814#M14081</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by deSteini on Tue Jun 03 11:56:42 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using an olimex LPC-P2919 board and since today, i cannot flash or program it anymore. I am using a Segger Jlink to flash it. I've tried to use the Tiny-H-Usb Tool to flash it, and since then it doesnt work anymore, not even the POWER-LED is on, only during i press the RESET BUTTON, or when i try to flash the Device. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;After that i get the error "bad jtag communication write to ir expected 0x1 got 0x7" &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;SPAN&gt;I saw the FAQ to &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fcontent%2Ffaq%2Flpcxpresso%2Fregaining-debug-access" rel="nofollow" target="_blank"&gt;http://www.lpcware.com/content/faq/lpcxpresso/regaining-debug-access&lt;/A&gt;&lt;SPAN&gt;, and i hope that would help, but i cannot find a ISP Pin for the 2919 and i found in another forum, that the LPC2919, doesnt have it...&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is that true, if yes, is there another possibility to regain access to debug? &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Its my second Board now who is in that mode, it would be great if i dont have to throw them away =)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;deSteini&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:50:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2919-not-able-to-program-anymore/m-p/550814#M14081</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:50:45Z</dc:date>
    </item>
    <item>
      <title>Re: LPC2919 not able to program anymore</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2919-not-able-to-program-anymore/m-p/550815#M14082</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by deSteini on Wed Jun 04 01:31:04 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I figured out that i am able to flash the Board with Keil, but not use the DebuggerMode in Keil. After the Flash, the Power LED works normal and the Code almost, too. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;But if i am going then back to the IAR Workbench and try to flash/debugg, i get the same problem as before, connection Problems and LED goes out...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Somebody has a hint?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:50:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2919-not-able-to-program-anymore/m-p/550815#M14082</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:50:46Z</dc:date>
    </item>
  </channel>
</rss>