<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックUSB0_VBUS connection for non-OTG devices?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB0-VBUS-connection-for-non-OTG-devices/m-p/550447#M14011</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by suckfish on Wed Sep 26 16:05:26 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;What's the easiest way to connect USB0_VBUS using the LPC43xx for a non-OTG USB device?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The user guide says that the pin is not 5v tolerant when VDDIO is not powered, but doesn't make a specific suggestion for connecting the pin.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The board is usb-powered, so under normal conditions, VDDIO will actually come up with a few milliseconds of usb being connected.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Looking a the Hitex eval board schematics, it connects USB0_VBUS directly to the usb connector (via only a ferrite bead).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Cheers,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ralph.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:34:11 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:34:11Z</dc:date>
    <item>
      <title>USB0_VBUS connection for non-OTG devices?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB0-VBUS-connection-for-non-OTG-devices/m-p/550447#M14011</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by suckfish on Wed Sep 26 16:05:26 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;What's the easiest way to connect USB0_VBUS using the LPC43xx for a non-OTG USB device?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The user guide says that the pin is not 5v tolerant when VDDIO is not powered, but doesn't make a specific suggestion for connecting the pin.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The board is usb-powered, so under normal conditions, VDDIO will actually come up with a few milliseconds of usb being connected.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Looking a the Hitex eval board schematics, it connects USB0_VBUS directly to the usb connector (via only a ferrite bead).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Cheers,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ralph.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:34:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB0-VBUS-connection-for-non-OTG-devices/m-p/550447#M14011</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:34:11Z</dc:date>
    </item>
    <item>
      <title>Re: USB0_VBUS connection for non-OTG devices?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB0-VBUS-connection-for-non-OTG-devices/m-p/550448#M14012</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Daniel Widyanto on Fri Sep 28 01:49:02 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Which LPC43xx datasheet that you use ? The USB_VBUS pin is 5V tolerant, and supposed to be connected directly to USB VBUS (+5V) to check whether the VBUS is there (for USB connection / disconnection event).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;SPAN&gt;The latest datasheet (&lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fdocuments%2Fdata_sheet%2FLPC4350_30_20_10.pdf" rel="nofollow" target="_blank"&gt;http://www.nxp.com/documents/data_sheet/LPC4350_30_20_10.pdf&lt;/A&gt;&lt;SPAN&gt;) shows that P2_5 is 5V tolerant &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:34:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB0-VBUS-connection-for-non-OTG-devices/m-p/550448#M14012</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:34:12Z</dc:date>
    </item>
    <item>
      <title>Re: USB0_VBUS connection for non-OTG devices?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB0-VBUS-connection-for-non-OTG-devices/m-p/550449#M14013</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by suckfish on Fri Sep 28 14:13:21 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I was looking at UM10503, which says on page 507:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;"The USB0_VBUS and USB1_VBUS pins are only 5 V tolerant when VDDIO is present.&amp;nbsp; Therefore, special precautions are necessary when the USB0 controller is implemented as a USB-powered USB device ...."&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:34:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB0-VBUS-connection-for-non-OTG-devices/m-p/550449#M14013</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:34:12Z</dc:date>
    </item>
    <item>
      <title>Re: USB0_VBUS connection for non-OTG devices?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB0-VBUS-connection-for-non-OTG-devices/m-p/550450#M14014</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Daniel Widyanto on Sun Sep 30 21:48:45 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Let me clarify this.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If your MCU VDD is available, but MCU VDDIO is not available, then you will have problem with the USB_VBUS pin (actually it's more like all of GPIO pins, coz the diode on the pin will not be turned on). That's what the sentence actually imposed.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If you tied your MCU VDD to the VDDIO, and USB_VBUS pin, the condition where the MCU VDD is available but VDDIO is not available will never happen. So, it's perfectly safe to connect all of these 3-pins to the USB Vbus without additional components. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Of course, I always recommend additional ESD diodes on each of USB pins (Vbus, D-, D+, GND) for better protection. But it's up to user to add it or not.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:34:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB0-VBUS-connection-for-non-OTG-devices/m-p/550450#M14014</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:34:13Z</dc:date>
    </item>
  </channel>
</rss>