<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC43xx sleep mode consumption</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-sleep-mode-consumption/m-p/550127#M13964</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ptamo on Mon Nov 10 16:09:18 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi nerd herd,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for your help, your results are interesting.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The manual says that sleep removes core clock, I do not understand why most of the core power consumption remains. This differs from my experiences in the past. LPC43xx are the first cortex-M I deal with, perhaps is something usual with this architecture.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Sleep mode current at the datasheet is specified&amp;nbsp; at 12Mhz IRC, so you must be right.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Your 84mA Active mode 204Mhz current measurement is far different from my measurements, this gives me hope.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have tested another of our boards with the LPC4330, this one from a different batch. I have modified my setup to get more precise current readings. I have tested my setup connecting a load to the LPC power rail (3.3v) to verify that my readings work.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Active mode current @204Mhz inside de while(1){} is 160mA higher than deep-sleep current. Deep-sleep current consumption is very similar to current consumption with the microcontroller at reset, this makes sense.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I understand that ResetISR is the first code executed at the micro. The user manual says that after a power-up the core clock BASE_M4_CLK is connected to the outputof PLL1 and running at 96 MHz and the clock source for the PLL1 is the 12 MHz IRC.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If I place a while(1){} loop at the first line of ResetISR current consumption is ~73mA, a datasheet graph states that at 96Mhz typical current consumption is ~40mA. Note that after a debug power up with the debuger attached BASE_M4_CLK is connected to the IRC an runs at 12Mhz.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Using crystal or IRC makes no significant difference.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have revised our schematics, comparing them to Keil MCB4300 development boards, looking for differences. I have moved some of the configuration pull resistors to test the jumper settings of the Keil development board. No changes found.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;We use LPCOpen v1.02 with some patches added. We have considered migrating our projects to newer v2 versions, but lots of changes are required.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;We use LPCXpresso and LPC-link2. Today I have migrated from LPCxpresso v7.1.1 to latest v7.5.0 version to see if it makes any difference on power consumption, no success.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Now I have run out of ideas.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;We run both LPC4330 and LPC4357 boards from batteries and power optimization is a must for us.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for your time&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Rubén&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:34:42 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:34:42Z</dc:date>
    <item>
      <title>LPC43xx sleep mode consumption</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-sleep-mode-consumption/m-p/550125#M13962</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ptamo on Fri Nov 07 07:21:32 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I use the LPC4330 in a custom board. It is clocked at 204Mhz and executing code from internal RAM.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am trying to reduce power consumption using the sleep mode whenever is possible. I have found that sleep mode reduces the total current consumption only 26mA. I believe that the power consumption reduction must at least 76mA as the datasheet specifies 81mA@204Mhz for the core in active mode and 5mA at sleep.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I use deep sleep mode in some situations were the microcontroller is not used and this mode reduces power consumption 180mA. If I reduce main clock to 102Mhz the consumption is halved, this seems coherent.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am sure that the microcontroller is entering sleep after the WFI instruction, I use a GPIO to monitor when it enters and leaves it.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;All current measurements are done without debugger attached and board power cycled after detaching debugger.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I can't mesure the total current consumption of the LPC alone as there are other peripherals at the board, but its current consumption must be more than 180mA. I find it too much considering that code is being executed from internal RAM. I mesure it inside a while(1){} with interrupts disabled. The only peripherals that are clocked are SSP0, SSP1, UART0 and the external memory controller, the rest of peripheral clocks are disabled.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;We use the LPC4357 in another custom board also clocked at 204Mhz. The sleep mode has the same effect. Current consumption is barely reduced.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My main doubts are:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-Is it normal that sleep mode only saves 26mA at 204Mhz?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-Is it normal that the LPC4330 executing a while(1){} from RAM drains more than 180mA?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This unanswered 2013 post seem to describe the same problem:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fcontent%2Fforum%2Flpc43xx-sleep-mode" rel="nofollow" target="_blank"&gt;http://www.lpcware.com/content/forum/lpc43xx-sleep-mode&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Rubén&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:34:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-sleep-mode-consumption/m-p/550125#M13962</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:34:40Z</dc:date>
    </item>
    <item>
      <title>Re: LPC43xx sleep mode consumption</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-sleep-mode-consumption/m-p/550126#M13963</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by nerd herd on Fri Nov 07 10:55:00 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi ptamo,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I did a quick test of the power consumption using an LPC4357 on the Keil MCB4300 development board using Keil uVision 5.12. I am measuring the current going into the chip to give you a better idea of the power savings to expect.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;After configuring things to save power, I enter an empty while(1) loop. This is with M0 core in reset state, -O0 optimization, with flash on (this should not matter since the delta between active mode and sleep mode is what matters):&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Active mode @ 204Mhz: 84.39 mA (2.9mA delta from the DS value with flash off)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Sleep mode @ 204MHz: 66.38 mA&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So it seems the difference between the two are the 20 or so mA you found. As for your comment about 5mA sleep current consumption, I believe that number is at 12MHz IRC.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Active mode @ 12MHz IRC:&amp;nbsp; 9.27 mA (2.7mA delta from DS value with flash off)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Sleep mode @ 12MHz: 7.94 mA&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So it seems that yes, sleep mode @ 204MHz saves the amount of power you are seeing, and that no, a while(1) from RAM should not consume 180mA.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:34:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-sleep-mode-consumption/m-p/550126#M13963</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:34:41Z</dc:date>
    </item>
    <item>
      <title>Re: LPC43xx sleep mode consumption</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-sleep-mode-consumption/m-p/550127#M13964</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ptamo on Mon Nov 10 16:09:18 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi nerd herd,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for your help, your results are interesting.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The manual says that sleep removes core clock, I do not understand why most of the core power consumption remains. This differs from my experiences in the past. LPC43xx are the first cortex-M I deal with, perhaps is something usual with this architecture.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Sleep mode current at the datasheet is specified&amp;nbsp; at 12Mhz IRC, so you must be right.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Your 84mA Active mode 204Mhz current measurement is far different from my measurements, this gives me hope.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have tested another of our boards with the LPC4330, this one from a different batch. I have modified my setup to get more precise current readings. I have tested my setup connecting a load to the LPC power rail (3.3v) to verify that my readings work.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Active mode current @204Mhz inside de while(1){} is 160mA higher than deep-sleep current. Deep-sleep current consumption is very similar to current consumption with the microcontroller at reset, this makes sense.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I understand that ResetISR is the first code executed at the micro. The user manual says that after a power-up the core clock BASE_M4_CLK is connected to the outputof PLL1 and running at 96 MHz and the clock source for the PLL1 is the 12 MHz IRC.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If I place a while(1){} loop at the first line of ResetISR current consumption is ~73mA, a datasheet graph states that at 96Mhz typical current consumption is ~40mA. Note that after a debug power up with the debuger attached BASE_M4_CLK is connected to the IRC an runs at 12Mhz.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Using crystal or IRC makes no significant difference.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have revised our schematics, comparing them to Keil MCB4300 development boards, looking for differences. I have moved some of the configuration pull resistors to test the jumper settings of the Keil development board. No changes found.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;We use LPCOpen v1.02 with some patches added. We have considered migrating our projects to newer v2 versions, but lots of changes are required.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;We use LPCXpresso and LPC-link2. Today I have migrated from LPCxpresso v7.1.1 to latest v7.5.0 version to see if it makes any difference on power consumption, no success.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Now I have run out of ideas.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;We run both LPC4330 and LPC4357 boards from batteries and power optimization is a must for us.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for your time&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Rubén&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:34:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-sleep-mode-consumption/m-p/550127#M13964</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:34:42Z</dc:date>
    </item>
    <item>
      <title>Re: LPC43xx sleep mode consumption</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-sleep-mode-consumption/m-p/550128#M13965</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Did this ever get resolved? We too have run a while(1) loop (running from flash) on the Keil&amp;nbsp;MCB4300 development board - and measured the potential across a shunt placed in the&amp;nbsp;Vddreg line (see mcb4300v1-3-schematics.pdf). At 204MHz, we measured currents of ~167mA (98mA at 102MHz).&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, we are using the LPCXpresso development environment. We’ve also performed similar current measurements on our own custom PCBs.&lt;/P&gt;&lt;P&gt;Is it possible that all the peripherals are actually on, and that we need to explicitly disable them? Do you have an example of your code that achieved the sub-90mA metric (Keil uvision example would be okay)&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Steve&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Mar 2017 09:58:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-sleep-mode-consumption/m-p/550128#M13965</guid>
      <dc:creator>stephencarey</dc:creator>
      <dc:date>2017-03-09T09:58:14Z</dc:date>
    </item>
  </channel>
</rss>