<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: some information on the chip_18x_43xx folder</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/some-information-on-the-chip-18x-43xx-folder/m-p/549138#M13777</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by xianghuiwang on Fri Aug 08 16:08:23 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi, pra18,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Source files under chip_18x_43xx folder should be able to be ported to your own custom lpc43xx board. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;They are however still sample programs, NXP does not assume any liability with the sample code. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Have a prefix of lpc_xxxx does not change the nature of the sample programs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;regards,&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:33:52 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:33:52Z</dc:date>
    <item>
      <title>some information on the chip_18x_43xx folder</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/some-information-on-the-chip-18x-43xx-folder/m-p/549137#M13776</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by pra18 on Tue Jul 29 03:45:43 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi, &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I need some information on the chip_18x_43xx folder in the lpcopen examples for ngx and hitex 4350 kits.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Are the sources inside these folder like clock_18xx_43xx.c/.h example implementation or to be used as it is ( NXP provided original sources)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;For example , I want to port the code into my own custom lpc43xx board , can I use these functions directly or are they jsut examples.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In which case which functions do I need to really use , does there exist a source file equivalent like lpc_xxxx.c given by nxp to use ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;or do I need to provide my own&amp;nbsp; functions &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance,&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:33:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/some-information-on-the-chip-18x-43xx-folder/m-p/549137#M13776</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:33:51Z</dc:date>
    </item>
    <item>
      <title>Re: some information on the chip_18x_43xx folder</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/some-information-on-the-chip-18x-43xx-folder/m-p/549138#M13777</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by xianghuiwang on Fri Aug 08 16:08:23 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi, pra18,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Source files under chip_18x_43xx folder should be able to be ported to your own custom lpc43xx board. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;They are however still sample programs, NXP does not assume any liability with the sample code. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Have a prefix of lpc_xxxx does not change the nature of the sample programs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;regards,&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:33:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/some-information-on-the-chip-18x-43xx-folder/m-p/549138#M13777</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:33:52Z</dc:date>
    </item>
  </channel>
</rss>