<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollersのトピックlpcopen bug</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpcopen-bug/m-p/548469#M13643</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lenguyen on Thu Mar 20 09:06:14 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi All,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am running into the issue to use Port 5 in LPC4088 however the&amp;nbsp; LPC_IOCON_T defined max as 5 ports instead of 6 ports.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;typedef struct {&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#if defined(CHIP_LPC175X_6X)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;__IO uint32_t PINSEL[11];&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;uint32_t RESERVED0[5];&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;__IO uint32_t PINMODE[10];&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;__IO uint32_t PINMODE_OD[5];&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;__IO uint32_t I2CPADCFG;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#else&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;__IO uint32_t p[5][32];&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#endif&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;} LPC_IOCON_T;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Am I missing something ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LN&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:31:58 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:31:58Z</dc:date>
    <item>
      <title>lpcopen bug</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpcopen-bug/m-p/548469#M13643</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lenguyen on Thu Mar 20 09:06:14 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi All,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am running into the issue to use Port 5 in LPC4088 however the&amp;nbsp; LPC_IOCON_T defined max as 5 ports instead of 6 ports.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;typedef struct {&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#if defined(CHIP_LPC175X_6X)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;__IO uint32_t PINSEL[11];&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;uint32_t RESERVED0[5];&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;__IO uint32_t PINMODE[10];&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;__IO uint32_t PINMODE_OD[5];&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;__IO uint32_t I2CPADCFG;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#else&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;__IO uint32_t p[5][32];&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#endif&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;} LPC_IOCON_T;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Am I missing something ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LN&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:31:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpcopen-bug/m-p/548469#M13643</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:31:58Z</dc:date>
    </item>
    <item>
      <title>Re: lpcopen bug</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpcopen-bug/m-p/548470#M13644</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by sundarapandian on Thu Mar 20 13:30:05 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you for pointing out the bug. Please use &lt;/SPAN&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;__IO uin32_t p[6][32];&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;SPAN&gt; instead of &lt;/SPAN&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;__IO uint32_t p[5][32];&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;SPAN&gt; this fix will be available with the next release.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:32:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpcopen-bug/m-p/548470#M13644</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:32:00Z</dc:date>
    </item>
  </channel>
</rss>