<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC4088 - IO configuration in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-IO-configuration/m-p/548374#M13637</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TKoe on Tue Mar 26 02:54:52 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've been reading the user manual for the 4088 and I've found some error in the part with the IO configuration.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;On page 141 all type W pins are listed: P0[7] to P0[9], P1[5] to P1[7], P[1]14 and P[1]16 to P[1]17.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;However, on page 140 only the pins on Port 0 are listed. The other pins are also not listed on page 130 (the pins that are not type D pins). They are also missing in the type D table.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am assuming that that is a copy/paste error from the LPC1788 and that the tables for the type D and W pins are correct (and only the descriptions are faulty) but can anyone confirm that?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best Regards!&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:32:37 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:32:37Z</dc:date>
    <item>
      <title>LPC4088 - IO configuration</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-IO-configuration/m-p/548374#M13637</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TKoe on Tue Mar 26 02:54:52 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've been reading the user manual for the 4088 and I've found some error in the part with the IO configuration.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;On page 141 all type W pins are listed: P0[7] to P0[9], P1[5] to P1[7], P[1]14 and P[1]16 to P[1]17.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;However, on page 140 only the pins on Port 0 are listed. The other pins are also not listed on page 130 (the pins that are not type D pins). They are also missing in the type D table.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am assuming that that is a copy/paste error from the LPC1788 and that the tables for the type D and W pins are correct (and only the descriptions are faulty) but can anyone confirm that?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best Regards!&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:32:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-IO-configuration/m-p/548374#M13637</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:32:37Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4088 - IO configuration</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-IO-configuration/m-p/548375#M13638</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by xianghuiwang on Fri Aug 30 14:46:43 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi, TKoe,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;You are correct!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Next UM release will have this fixed.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;regard,&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:32:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-IO-configuration/m-p/548375#M13638</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:32:38Z</dc:date>
    </item>
  </channel>
</rss>