<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPC2362 Not entering ISP mode</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2362-Not-entering-ISP-mode/m-p/548360#M13635</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jaisankar_av on Thu Jul 04 00:05:01 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;I have a strange problem with my board LPC2362. The fresh controller is getting programmed for the very first time. And the second time onwards the controller is not entering into ISP mode.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;I am using Flash magic for programming. RTS and CTS are included in the ISP connections and using via PC serial port.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;I have probed the Reset pin and EINT(P2.10). Both are going LOW initially and then HIGH when trying to connect from flash magic, though not connecting on second attempt. The error I get is Failed to Autobaud.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;First time after changing the controller, it works fine. So the ISP circuit is fine I guess.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Any valuable suggessions would be highly appriciated.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:51:01 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:51:01Z</dc:date>
    <item>
      <title>LPC2362 Not entering ISP mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2362-Not-entering-ISP-mode/m-p/548360#M13635</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jaisankar_av on Thu Jul 04 00:05:01 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;I have a strange problem with my board LPC2362. The fresh controller is getting programmed for the very first time. And the second time onwards the controller is not entering into ISP mode.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;I am using Flash magic for programming. RTS and CTS are included in the ISP connections and using via PC serial port.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;I have probed the Reset pin and EINT(P2.10). Both are going LOW initially and then HIGH when trying to connect from flash magic, though not connecting on second attempt. The error I get is Failed to Autobaud.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;First time after changing the controller, it works fine. So the ISP circuit is fine I guess.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Any valuable suggessions would be highly appriciated.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:51:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2362-Not-entering-ISP-mode/m-p/548360#M13635</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:51:01Z</dc:date>
    </item>
    <item>
      <title>Re: LPC2362 Not entering ISP mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2362-Not-entering-ISP-mode/m-p/548361#M13636</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by barny on Wed Dec 04 01:49:26 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have also experienced this! When there is no code in the processor, it will automatically go into bootloader mode, that is why you can load first time.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I don't think the problem is flash Magic, but the RESET pin on the processor is not being seen.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have also made a post to see if anyone is aware of a RESET issue.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:51:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2362-Not-entering-ISP-mode/m-p/548361#M13636</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:51:02Z</dc:date>
    </item>
  </channel>
</rss>