<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Interesting behavior on LPC4088 Quickstart board + Experiment Base Board (Network related) in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Interesting-behavior-on-LPC4088-Quickstart-board-Experiment-Base/m-p/548303#M13619</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by profanum429 on Fri Apr 03 18:34:27 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;We have a LPC4088 QSB + associated Experiment Base Board. We've been running a LPCOpen based network application on one of them for the past 2 months without issue and ordered three more QSBs + base boards. These three arrived and all exhibit the same issue; when we do a cold start we'll see the PHY immediately think it has a connection (polling the PHY status initially returns 0x02 then constantly 0x3C immediately after). This behavior happens wether a cable is plugged in or not. Pressing the reset button results in normal expected behavior that our original setup produces.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Removing power completely and doing another cold start brings back the original problem which can be solved by the user doing a reset. Doing a NVIC_SystemReset does not fix the issue nor does connecting a GPIO to the reset line and pulling it high in software. I'm assuming this is an issue with the LAN8720 needing to have a 100 uSec reset time and my software reset strategies don't produce nearly that amount of time.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I also see this same issue using the tcpecho_sa sample project from the 2.10 version of LPCOpen for the LPC4088. I'm wondering if anyone else has seen this issue? I'm thinking we might of gotten a set of QSBs (the ones with the problem all have the same lot and date code, different from the working one) that might have a defective component? Next step will probably be monitoring the power signal going to the LAN8720 on startup on a bad board and a good board but that will have to wait until Monday.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:30:29 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:30:29Z</dc:date>
    <item>
      <title>Interesting behavior on LPC4088 Quickstart board + Experiment Base Board (Network related)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Interesting-behavior-on-LPC4088-Quickstart-board-Experiment-Base/m-p/548303#M13619</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by profanum429 on Fri Apr 03 18:34:27 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;We have a LPC4088 QSB + associated Experiment Base Board. We've been running a LPCOpen based network application on one of them for the past 2 months without issue and ordered three more QSBs + base boards. These three arrived and all exhibit the same issue; when we do a cold start we'll see the PHY immediately think it has a connection (polling the PHY status initially returns 0x02 then constantly 0x3C immediately after). This behavior happens wether a cable is plugged in or not. Pressing the reset button results in normal expected behavior that our original setup produces.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Removing power completely and doing another cold start brings back the original problem which can be solved by the user doing a reset. Doing a NVIC_SystemReset does not fix the issue nor does connecting a GPIO to the reset line and pulling it high in software. I'm assuming this is an issue with the LAN8720 needing to have a 100 uSec reset time and my software reset strategies don't produce nearly that amount of time.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I also see this same issue using the tcpecho_sa sample project from the 2.10 version of LPCOpen for the LPC4088. I'm wondering if anyone else has seen this issue? I'm thinking we might of gotten a set of QSBs (the ones with the problem all have the same lot and date code, different from the working one) that might have a defective component? Next step will probably be monitoring the power signal going to the LAN8720 on startup on a bad board and a good board but that will have to wait until Monday.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:30:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Interesting-behavior-on-LPC4088-Quickstart-board-Experiment-Base/m-p/548303#M13619</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:30:29Z</dc:date>
    </item>
    <item>
      <title>Re: Interesting behavior on LPC4088 Quickstart board + Experiment Base Board (Network related)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Interesting-behavior-on-LPC4088-Quickstart-board-Experiment-Base/m-p/548304#M13620</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by xianghuiwang on Fri Apr 24 10:38:22 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;hi, &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;your observation makes a lot sense. Thanks for letting us know.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Please keep us posted with your findings.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:30:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Interesting-behavior-on-LPC4088-Quickstart-board-Experiment-Base/m-p/548304#M13620</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:30:31Z</dc:date>
    </item>
  </channel>
</rss>