<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC4088 and TFTs in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-and-TFTs/m-p/547850#M13542</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mulfycrowh on Sun Jan 17 07:58:14 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi everyone !&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using LPC4088.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The question is about hardware development and more precisely how to select the pins of the LPC4088.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;EMC pins are used in my development for external flash and sram.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I would like to add a LCD screen 24 bits.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The idea is to use LCD_VD[0...23] pins. I noticed that all these pins are declared in the datasheet as outputs except LCD_VD[3] and LCD_VD[7] that are inputs on pin P2.9.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Why inputs ? Is there a mistake in the datasheet ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Data bus for TFTs is made of outputs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Can I use P2.9 as an output for LCD purpose ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Many thanks for help&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:31:32 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:31:32Z</dc:date>
    <item>
      <title>LPC4088 and TFTs</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-and-TFTs/m-p/547850#M13542</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mulfycrowh on Sun Jan 17 07:58:14 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi everyone !&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using LPC4088.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The question is about hardware development and more precisely how to select the pins of the LPC4088.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;EMC pins are used in my development for external flash and sram.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I would like to add a LCD screen 24 bits.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The idea is to use LCD_VD[0...23] pins. I noticed that all these pins are declared in the datasheet as outputs except LCD_VD[3] and LCD_VD[7] that are inputs on pin P2.9.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Why inputs ? Is there a mistake in the datasheet ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Data bus for TFTs is made of outputs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Can I use P2.9 as an output for LCD purpose ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Many thanks for help&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:31:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-and-TFTs/m-p/547850#M13542</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:31:32Z</dc:date>
    </item>
  </channel>
</rss>