<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックNo current flowing in GPIO pin?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/No-current-flowing-in-GPIO-pin/m-p/547512#M13492</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by DodigI on Sun Jun 08 04:12:01 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello, can someone please explain this phenomena.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;A GPIO pin is set as input with pull-up resistor enabled. Power supply is 3.3V. When I short the pin to ground a current of 55uA (60kR calculated pull-up value) is flowing through the pull-up resistor.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;However, if I apply a 5V to the pin no current is flowing into the pin?! I would expect a current of ((5V-3.3V)/60kR) to flow, but I measure only 1nA (measured with a very precise source measure unit).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What is the catch here? I'm trying to understand how the ESD protection and 5V tolerant inputs work.. When the pull-up is disabled no current is flowing also, which makes sense if the pins are really 5V tolerant. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:47:31 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:47:31Z</dc:date>
    <item>
      <title>No current flowing in GPIO pin?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/No-current-flowing-in-GPIO-pin/m-p/547512#M13492</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by DodigI on Sun Jun 08 04:12:01 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello, can someone please explain this phenomena.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;A GPIO pin is set as input with pull-up resistor enabled. Power supply is 3.3V. When I short the pin to ground a current of 55uA (60kR calculated pull-up value) is flowing through the pull-up resistor.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;However, if I apply a 5V to the pin no current is flowing into the pin?! I would expect a current of ((5V-3.3V)/60kR) to flow, but I measure only 1nA (measured with a very precise source measure unit).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What is the catch here? I'm trying to understand how the ESD protection and 5V tolerant inputs work.. When the pull-up is disabled no current is flowing also, which makes sense if the pins are really 5V tolerant. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:47:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/No-current-flowing-in-GPIO-pin/m-p/547512#M13492</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:47:31Z</dc:date>
    </item>
    <item>
      <title>Re: No current flowing in GPIO pin?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/No-current-flowing-in-GPIO-pin/m-p/547513#M13493</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by 1234567890 on Mon Jun 09 00:20:09 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The reason ist that the pull-x are no real resistors:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fcontent%2Fforum%2Flpc1114-pull-updown-resistors-value" rel="nofollow" target="_blank"&gt;http://www.lpcware.com/content/forum/lpc1114-pull-updown-resistors-value&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fcontent%2Fforum%2Finternal-pull-resistors" rel="nofollow" target="_blank"&gt;http://www.lpcware.com/content/forum/internal-pull-resistors&lt;/A&gt;&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:47:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/No-current-flowing-in-GPIO-pin/m-p/547513#M13493</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:47:31Z</dc:date>
    </item>
  </channel>
</rss>