<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: FreeRTOS under Crossworks for ARM</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/FreeRTOS-under-Crossworks-for-ARM/m-p/547365#M13472</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TheFallGuy on Thu Jul 31 01:28:02 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;AFAIK, Crossworks uses GCC, so provided you use a GCC port of FreeRTOS it should build. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;FreeRTOS doesn't know or need to know anything about the board - only the ARM core you are using. So use a Cortex-M4 port of FreeRTOS for the GCC toolchain.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If that doesn't help, ask on the FreeRTOS forums.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:29:49 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:29:49Z</dc:date>
    <item>
      <title>FreeRTOS under Crossworks for ARM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/FreeRTOS-under-Crossworks-for-ARM/m-p/547364#M13471</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by paul.rcom-software.com on Wed Jul 30 10:39:11 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Folks:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does anybody know where to obtain a port of FreeRTOS that runs&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;on the Embedded Artists&amp;nbsp; LCP4088-32&amp;nbsp; board and can be built&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;with Rowley Crossworks for ARM ?&amp;nbsp; Rowley sometimes refers&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;to&amp;nbsp; LPC4088 support as LPC1000 support--somewhat confusingly.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Also, I think, floating point hardware support is the default option&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;which is fine in my case.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:29:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/FreeRTOS-under-Crossworks-for-ARM/m-p/547364#M13471</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:29:48Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS under Crossworks for ARM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/FreeRTOS-under-Crossworks-for-ARM/m-p/547365#M13472</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TheFallGuy on Thu Jul 31 01:28:02 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;AFAIK, Crossworks uses GCC, so provided you use a GCC port of FreeRTOS it should build. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;FreeRTOS doesn't know or need to know anything about the board - only the ARM core you are using. So use a Cortex-M4 port of FreeRTOS for the GCC toolchain.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If that doesn't help, ask on the FreeRTOS forums.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:29:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/FreeRTOS-under-Crossworks-for-ARM/m-p/547365#M13472</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:29:49Z</dc:date>
    </item>
  </channel>
</rss>