<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC4088 with SPIFI FLASH Above 16MB/24 Bit</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-with-SPIFI-FLASH-Above-16MB-24-Bit/m-p/547210#M13452</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The software interface to the SPIFI controller is the same as for the LPC43xx parts so I can see no reason why this would not work - however I have not actually tried this.&amp;nbsp; Of course regardless, only 16MBs will be accessible from code running on the LPC4088.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yours,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;LPCXpresso-support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Aug 2016 08:52:31 GMT</pubDate>
    <dc:creator>lpcxpresso_supp</dc:creator>
    <dc:date>2016-08-19T08:52:31Z</dc:date>
    <item>
      <title>LPC4088 with SPIFI FLASH Above 16MB/24 Bit</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-with-SPIFI-FLASH-Above-16MB-24-Bit/m-p/547207#M13449</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by schibli on Fri Jan 09 06:03:07 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Can LPC408x support more than 16MB of SPIFI SPI flash memory with the newest version of SPIFILIB (V1.01), &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;or is it a matter of hardware (24 Bit addressing limit, SPIFI Buffer Space 0x2800 0000 - 0x28FF FFFF)?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:32:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-with-SPIFI-FLASH-Above-16MB-24-Bit/m-p/547207#M13449</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:32:44Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4088 with SPIFI FLASH Above 16MB/24 Bit</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-with-SPIFI-FLASH-Above-16MB-24-Bit/m-p/547208#M13450</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mc on Sat Jan 10 07:43:56 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi schibli,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC4088 supports only up to 16MB SPIFI flash memory mapped area. LPC1800/4300 devices support more than 16MB SPIFI flash memory. SPIFI hardware supports more than 3 bytes addressing. It was not implemented in new SPIFI library. We will implement it. It has been implemented in old version of SPIFI library.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:32:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-with-SPIFI-FLASH-Above-16MB-24-Bit/m-p/547208#M13450</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:32:45Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4088 with SPIFI FLASH Above 16MB/24 Bit</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-with-SPIFI-FLASH-Above-16MB-24-Bit/m-p/547209#M13451</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can SPIFI flash greater than 16MB be used in Command mode?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Aug 2016 17:28:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-with-SPIFI-FLASH-Above-16MB-24-Bit/m-p/547209#M13451</guid>
      <dc:creator>hungmai</dc:creator>
      <dc:date>2016-08-18T17:28:03Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4088 with SPIFI FLASH Above 16MB/24 Bit</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-with-SPIFI-FLASH-Above-16MB-24-Bit/m-p/547210#M13452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The software interface to the SPIFI controller is the same as for the LPC43xx parts so I can see no reason why this would not work - however I have not actually tried this.&amp;nbsp; Of course regardless, only 16MBs will be accessible from code running on the LPC4088.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yours,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;LPCXpresso-support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Aug 2016 08:52:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-with-SPIFI-FLASH-Above-16MB-24-Bit/m-p/547210#M13452</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2016-08-19T08:52:31Z</dc:date>
    </item>
  </channel>
</rss>