<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Pull-ups Enabled on RESET</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Pull-ups-Enabled-on-RESET/m-p/546868#M13350</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by larsen on Fri Jun 21 13:15:44 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;Can you add an inverter chip on the output. I see no other way.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:48:03 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:48:03Z</dc:date>
    <item>
      <title>Pull-ups Enabled on RESET</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Pull-ups-Enabled-on-RESET/m-p/546867#M13349</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by neilt6 on Wed Jun 12 10:15:54 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;Hey guys. I'm getting progressively more irritated with the fact that pullup resistors are enabled by default on this LPC11U35 I'm playing with. Here's my situation: I'm building a battery powered device that has several active-high outputs that I need to hold low until my software is up and running (LDO enable, charger enable, etc). This becomes an even bigger issue when I try to use the USB bootloader for firmware updates. In this case, there's no way to shut the system off, because the pullup keeps the regulator enabled! How do you guys overcome this issue? I can use a strong pulldown resistor on these outputs, but that directly affects battery life.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:48:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Pull-ups-Enabled-on-RESET/m-p/546867#M13349</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:48:02Z</dc:date>
    </item>
    <item>
      <title>Re: Pull-ups Enabled on RESET</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Pull-ups-Enabled-on-RESET/m-p/546868#M13350</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by larsen on Fri Jun 21 13:15:44 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;Can you add an inverter chip on the output. I see no other way.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:48:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Pull-ups-Enabled-on-RESET/m-p/546868#M13350</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:48:03Z</dc:date>
    </item>
    <item>
      <title>Re: Pull-ups Enabled on RESET</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Pull-ups-Enabled-on-RESET/m-p/546869#M13351</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by neilt6 on Tue Jul 02 19:09:27 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Unfortunately no, my boss wants to keep the BOM as short as possible, and 10KΩ pull-downs are cheaper than inverters...&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:48:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Pull-ups-Enabled-on-RESET/m-p/546869#M13351</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:48:04Z</dc:date>
    </item>
  </channel>
</rss>