<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: replace watchdog oscillator with ext osc</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/replace-watchdog-oscillator-with-ext-osc/m-p/546847#M13346</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by nxp_apps on Fri Jan 16 11:00:45 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Theodore,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Sorry, but for deep sleep mode, you can not use an external clock.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;NXP Support&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:46:40 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:46:40Z</dc:date>
    <item>
      <title>replace watchdog oscillator with ext osc</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/replace-watchdog-oscillator-with-ext-osc/m-p/546846#M13345</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by tbelo on Sat Dec 13 03:42:29 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Trimming my prototype board with the "timed wakeup" application scenario had pretty good wakeup times.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Testing the same code with the production boards I realize the in each board the wakeup time varies &lt;/SPAN&gt;&lt;STRONG&gt;unacceptable&lt;/STRONG&gt;&lt;SPAN&gt; for the application.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Since I haven't used any external oscillator can I attach an external one to replace watchdog oscillator for the deep sleep timing ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;And if yes with what characteristics for my low power application?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I use lpc1115.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I see that in user manual manual but just wondering if I can save the project somehow:&lt;/SPAN&gt;&lt;BR /&gt;&lt;STRONG&gt;3.9.3.1 Power configuration in Deep-sleep mode&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Power consumption in Deep-sleep mode is determined by the Deep-sleep power&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;configuration setting in the PDSLEEPCFG (Table 41) register:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;• &lt;/SPAN&gt;&lt;STRONG&gt;The only clock source available in Deep-sleep mode is the watchdog oscillator&lt;/STRONG&gt;&lt;SPAN&gt;. The&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;watchdog oscillator can be left running in Deep-sleep mode if required for&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;timer-controlled wake-up (see Section 3.10.3). All other clock sources (the IRC and&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;system oscillator) and the system PLL are shut down. The watchdog oscillator analog&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;output frequency must be set to the lowest value of its analog clock output (bits&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;FREQSEL in the WDTOSCCTRL = 0001, see Table 13).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best regards&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:46:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/replace-watchdog-oscillator-with-ext-osc/m-p/546846#M13345</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:46:39Z</dc:date>
    </item>
    <item>
      <title>Re: replace watchdog oscillator with ext osc</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/replace-watchdog-oscillator-with-ext-osc/m-p/546847#M13346</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by nxp_apps on Fri Jan 16 11:00:45 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Theodore,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Sorry, but for deep sleep mode, you can not use an external clock.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;NXP Support&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:46:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/replace-watchdog-oscillator-with-ext-osc/m-p/546847#M13346</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:46:40Z</dc:date>
    </item>
  </channel>
</rss>