<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: timer overflow checking?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/timer-overflow-checking/m-p/546747#M13324</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Prayook,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The timer can only generate interrupts on match or capture events, the overflow event does not cause an interrupt, but a match register can be used to detect an overflow if needed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Carlos Mendoza&lt;/P&gt;&lt;P&gt;Technical Support Engineer&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Jul 2016 16:26:18 GMT</pubDate>
    <dc:creator>Carlos_Mendoza</dc:creator>
    <dc:date>2016-07-19T16:26:18Z</dc:date>
    <item>
      <title>timer overflow checking?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/timer-overflow-checking/m-p/546746#M13323</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm working on LPC54102 and I use timestamp from StopWatch_Start() which return 32 bit data.&lt;/P&gt;&lt;P&gt;How do I know when the time overflow happen? Is there any interrupt for that?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jul 2016 15:49:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/timer-overflow-checking/m-p/546746#M13323</guid>
      <dc:creator>koonyook</dc:creator>
      <dc:date>2016-07-07T15:49:50Z</dc:date>
    </item>
    <item>
      <title>Re: timer overflow checking?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/timer-overflow-checking/m-p/546747#M13324</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Prayook,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The timer can only generate interrupts on match or capture events, the overflow event does not cause an interrupt, but a match register can be used to detect an overflow if needed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Carlos Mendoza&lt;/P&gt;&lt;P&gt;Technical Support Engineer&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jul 2016 16:26:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/timer-overflow-checking/m-p/546747#M13324</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2016-07-19T16:26:18Z</dc:date>
    </item>
  </channel>
</rss>