<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: VC++ project files for emwin</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/VC-project-files-for-emwin/m-p/546458#M13267</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by drs on Thu May 17 06:32:55 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;They should be in the base directory of the BSPs. They are called simulation.sln and simulation.vcxproj.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:29:08 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:29:08Z</dc:date>
    <item>
      <title>VC++ project files for emwin</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/VC-project-files-for-emwin/m-p/546457#M13266</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ravi Teja on Thu May 17 03:15:12 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; For emwin graphics library they mentioned about VC++ project files but they didn't given any VC++ project files in both the libraries and BSP . IS it a paid service or we can get for free? In the BSP which we have downloaded the following path NXP\emWin\Start\Sample\Tutorial contains so many example problems are we have to run these problems using VC++ for that no project files they have given.Where we can get these&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:29:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/VC-project-files-for-emwin/m-p/546457#M13266</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:29:07Z</dc:date>
    </item>
    <item>
      <title>Re: VC++ project files for emwin</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/VC-project-files-for-emwin/m-p/546458#M13267</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by drs on Thu May 17 06:32:55 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;They should be in the base directory of the BSPs. They are called simulation.sln and simulation.vcxproj.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:29:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/VC-project-files-for-emwin/m-p/546458#M13267</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:29:08Z</dc:date>
    </item>
  </channel>
</rss>