<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Sample Code for Using Both USB Ports as Host Simultaneously in LPC2468 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Sample-Code-for-Using-Both-USB-Ports-as-Host-Simultaneously-in/m-p/546451#M13263</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by simersarao on Mon Mar 21 04:15:36 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am Using LPC2468 in my ECR machine. I have successfully interfaced USB Pendrive,USB Printer and USB bar-code Scanner with the Micro-controller. But the Problem is that most use cases require both USB Printer and Bar-code scanner to work simultaneously, but I can only use one device at a time due to only single USB Host port Functional.After Researching a lot on Web I have not found any link or sample code which allows both Ports (i.e Dedicated USB Host port and OTG one) to be used simultaneously.Please provide some sample source code or&amp;nbsp; some help material using which i should be able to configure and use both USB ports as Host simultaneously. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Simer&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:50:01 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:50:01Z</dc:date>
    <item>
      <title>Sample Code for Using Both USB Ports as Host Simultaneously in LPC2468</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Sample-Code-for-Using-Both-USB-Ports-as-Host-Simultaneously-in/m-p/546451#M13263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by simersarao on Mon Mar 21 04:15:36 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am Using LPC2468 in my ECR machine. I have successfully interfaced USB Pendrive,USB Printer and USB bar-code Scanner with the Micro-controller. But the Problem is that most use cases require both USB Printer and Bar-code scanner to work simultaneously, but I can only use one device at a time due to only single USB Host port Functional.After Researching a lot on Web I have not found any link or sample code which allows both Ports (i.e Dedicated USB Host port and OTG one) to be used simultaneously.Please provide some sample source code or&amp;nbsp; some help material using which i should be able to configure and use both USB ports as Host simultaneously. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Simer&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:50:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Sample-Code-for-Using-Both-USB-Ports-as-Host-Simultaneously-in/m-p/546451#M13263</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:50:01Z</dc:date>
    </item>
    <item>
      <title>Re: Sample Code for Using Both USB Ports as Host Simultaneously in LPC2468</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Sample-Code-for-Using-Both-USB-Ports-as-Host-Simultaneously-in/m-p/546452#M13264</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Jat on Thu Mar 24 09:26:29 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Simer&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am glad that you raised the question, I have also been in a similar situation with LPC1788 and was thinking to try myself on the code.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Have you tried changing the example codes, and if so then what issues are you facing?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:50:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Sample-Code-for-Using-Both-USB-Ports-as-Host-Simultaneously-in/m-p/546452#M13264</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:50:01Z</dc:date>
    </item>
    <item>
      <title>Re: Sample Code for Using Both USB Ports as Host Simultaneously in LPC2468</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Sample-Code-for-Using-Both-USB-Ports-as-Host-Simultaneously-in/m-p/546453#M13265</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;bump&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Jun 2016 01:05:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Sample-Code-for-Using-Both-USB-Ports-as-Host-Simultaneously-in/m-p/546453#M13265</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-19T01:05:57Z</dc:date>
    </item>
  </channel>
</rss>