<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC 4337 - Any constraints on simultaneous AHB transfers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-4337-Any-constraints-on-simultaneous-AHB-transfers/m-p/546386#M13250</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jackgeotech on Thu Apr 02 10:48:20 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'd appreciate an authoritative answer to a question about the AHB bus on the LPC4337.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The diagram "AHB multilayer matrix master and slave connections" - Fig. 11 in the UM10503 - implies that there are no constraints or arbitration delays on bus transfers as long as each peripheral group is accessed by only one master at any given time.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;For greater clarity, in the LPC4337 (which has no Subsys M0 core) there are 11 masters and 11 slaves.&amp;nbsp; So in an extreme case, each of the 11 masters could be accessing a different slave, all at the same time, and there should be no conflict or arbitration delays.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have assumed that this is true, but I have not been able to find an unequivocal statement in the NXP documentation.&amp;nbsp; For some of the other NXP chips it is clearly stated that there are no arbitration delays as long as two masters don't try to access the same slave.&amp;nbsp; I have not been able to find a similar statement for the LPC43xx.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Out of curiosity, what is it that is "multilayer" about the "AHB multilayer matrix"?&amp;nbsp; I don't see multiple layers in Fig.11.&amp;nbsp; So I'm wondering if the real structure is more complex than shown in Fig. 11, possibly introducing some constraints.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:31:30 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:31:30Z</dc:date>
    <item>
      <title>LPC 4337 - Any constraints on simultaneous AHB transfers</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-4337-Any-constraints-on-simultaneous-AHB-transfers/m-p/546386#M13250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jackgeotech on Thu Apr 02 10:48:20 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'd appreciate an authoritative answer to a question about the AHB bus on the LPC4337.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The diagram "AHB multilayer matrix master and slave connections" - Fig. 11 in the UM10503 - implies that there are no constraints or arbitration delays on bus transfers as long as each peripheral group is accessed by only one master at any given time.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;For greater clarity, in the LPC4337 (which has no Subsys M0 core) there are 11 masters and 11 slaves.&amp;nbsp; So in an extreme case, each of the 11 masters could be accessing a different slave, all at the same time, and there should be no conflict or arbitration delays.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have assumed that this is true, but I have not been able to find an unequivocal statement in the NXP documentation.&amp;nbsp; For some of the other NXP chips it is clearly stated that there are no arbitration delays as long as two masters don't try to access the same slave.&amp;nbsp; I have not been able to find a similar statement for the LPC43xx.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Out of curiosity, what is it that is "multilayer" about the "AHB multilayer matrix"?&amp;nbsp; I don't see multiple layers in Fig.11.&amp;nbsp; So I'm wondering if the real structure is more complex than shown in Fig. 11, possibly introducing some constraints.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:31:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-4337-Any-constraints-on-simultaneous-AHB-transfers/m-p/546386#M13250</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:31:30Z</dc:date>
    </item>
  </channel>
</rss>