<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: UART3 on lpc40XX parts</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/UART3-on-lpc40XX-parts/m-p/546050#M13177</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by schisanoa on Mon Jan 20 08:38:43 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I've now receivd the answer from NXP technical support( very fast answer, very efficient)!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'll report:&lt;/SPAN&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;The pins have multiplexers which allows to connect several functions to a single pin. Which function is active can be selected through the IOCON register. This is explained in the UM (www.nxp.com/documents/user_manual/UM10562.pdf), chapter 'Chapter 7: LPC408x/407x I/O configuration'&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Now the problem is only on the PINMUX application. Someone know if it possible to manage the problem on the app?(it is useful if possible)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks at all&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Alessio&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:29:46 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:29:46Z</dc:date>
    <item>
      <title>UART3 on lpc40XX parts</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/UART3-on-lpc40XX-parts/m-p/546049#M13176</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by schisanoa on Mon Jan 20 07:48:46 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Looking at the DS I see that UART 3 is assigned at too much PIN, U3TX and U3RX are mapped on:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;P0.0 and P0.1&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;P0.2 and P0.3&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;P0.25 and P0.26&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;P4.28 and P4.29&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;in addition UART0 is also mapped on too much PIN, &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;P0.0 and P0.1&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;P0.2 and P0.3&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using Rev. 2 — 3 July 2013 datasheet downloaded from NXP web site, on the LPC4078 page 4 or 5 days ago. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Has someone an updated datasheet to share with me?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I would also advise the other user that PINMUX application for LPC40xx is affected from this problem, in order to avoid some trouble to someone.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Alessio&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;PS: I've already check the ERRATA docs, but nothing is reported&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:29:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/UART3-on-lpc40XX-parts/m-p/546049#M13176</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:29:45Z</dc:date>
    </item>
    <item>
      <title>Re: UART3 on lpc40XX parts</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/UART3-on-lpc40XX-parts/m-p/546050#M13177</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by schisanoa on Mon Jan 20 08:38:43 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I've now receivd the answer from NXP technical support( very fast answer, very efficient)!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'll report:&lt;/SPAN&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;The pins have multiplexers which allows to connect several functions to a single pin. Which function is active can be selected through the IOCON register. This is explained in the UM (www.nxp.com/documents/user_manual/UM10562.pdf), chapter 'Chapter 7: LPC408x/407x I/O configuration'&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Now the problem is only on the PINMUX application. Someone know if it possible to manage the problem on the app?(it is useful if possible)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks at all&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Alessio&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:29:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/UART3-on-lpc40XX-parts/m-p/546050#M13177</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:29:46Z</dc:date>
    </item>
  </channel>
</rss>