<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic VDD pins in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/VDD-pins/m-p/545775#M13125</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by IanB on Sat Dec 20 09:27:01 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I don't think it says in the data sheet that BOTH Vdd pins must be connected for the IC to function - if it does, then I can't find it.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I've just found out the hard way! (and, I've also found out that attaching a wire to one pin of a FHN33 package is also just a little tricky!)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;A quick test with a continuity tester shows that pin 6 is not connected to pin 29 on the FHN33 package.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If this is the case, then how should I interpret the limiting values for Idd in the data sheet - it says "100mA maximum &lt;/SPAN&gt;&lt;I&gt;per supply pin&lt;/I&gt;&lt;SPAN&gt;". If various parts of the IC are supplied from the two different pins, how would I which Vdd pins was supplying the load?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:46:40 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:46:40Z</dc:date>
    <item>
      <title>VDD pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/VDD-pins/m-p/545775#M13125</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by IanB on Sat Dec 20 09:27:01 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I don't think it says in the data sheet that BOTH Vdd pins must be connected for the IC to function - if it does, then I can't find it.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I've just found out the hard way! (and, I've also found out that attaching a wire to one pin of a FHN33 package is also just a little tricky!)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;A quick test with a continuity tester shows that pin 6 is not connected to pin 29 on the FHN33 package.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If this is the case, then how should I interpret the limiting values for Idd in the data sheet - it says "100mA maximum &lt;/SPAN&gt;&lt;I&gt;per supply pin&lt;/I&gt;&lt;SPAN&gt;". If various parts of the IC are supplied from the two different pins, how would I which Vdd pins was supplying the load?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:46:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/VDD-pins/m-p/545775#M13125</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:46:40Z</dc:date>
    </item>
  </channel>
</rss>