<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 GPDMA to I2S peripheral questions</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/GPDMA-to-I2S-peripheral-questions/m-p/545704#M13119</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jdowd on Thu Nov 20 14:21:59 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a memory buffer with audio data in it that I want to move to the Transmit side of the I2S peripheral. I have this done using a more conventional method (straight copy using ring buffers, works great!!) but I want to introduce the GPDMA feature.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;For the flow control, am I correct in assuming that the I2S side can perform the flow control since it has a FIFO and does report it's current data level?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Also, for interrupts, I would think that there is just a GPDMA interrupt to service (TC &amp;amp; Error) since the peripheral (via it's flow control) would handle the constant bursts required to keep the I2S FIFO fed until the memory buffer was emtpy. Correct?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The example in periph_i2s does have a GPDMA example except that it's a straight Peripheral - Peripheral transfer. Not from memory although it has been a great source of information.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance for any advice you can render.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Cheers!!&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:29:59 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:29:59Z</dc:date>
    <item>
      <title>GPDMA to I2S peripheral questions</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/GPDMA-to-I2S-peripheral-questions/m-p/545704#M13119</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jdowd on Thu Nov 20 14:21:59 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a memory buffer with audio data in it that I want to move to the Transmit side of the I2S peripheral. I have this done using a more conventional method (straight copy using ring buffers, works great!!) but I want to introduce the GPDMA feature.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;For the flow control, am I correct in assuming that the I2S side can perform the flow control since it has a FIFO and does report it's current data level?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Also, for interrupts, I would think that there is just a GPDMA interrupt to service (TC &amp;amp; Error) since the peripheral (via it's flow control) would handle the constant bursts required to keep the I2S FIFO fed until the memory buffer was emtpy. Correct?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The example in periph_i2s does have a GPDMA example except that it's a straight Peripheral - Peripheral transfer. Not from memory although it has been a great source of information.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance for any advice you can render.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Cheers!!&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:29:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/GPDMA-to-I2S-peripheral-questions/m-p/545704#M13119</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:29:59Z</dc:date>
    </item>
  </channel>
</rss>