<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to deploy application to phytec developement board running with NXP WinCE BSP in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-deploy-application-to-phytec-developement-board-running/m-p/544231#M12858</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by rcsison on Wed Jul 18 18:49:35 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;In the Platform Building, we have two things selected in the Catalog Items:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Under Core OS-&amp;gt;Applications - End User, we have "ActiveSync" selected.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Under Third Party-&amp;gt;BSP-&amp;gt;PhyCore_LPC3250: ARMV4I-&amp;gt;USB Drivers, we have "USB Device Driver" selected so ActiveSync will work. "USB Host Driver" is for giving the device the capability to read a USB memory stick.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;A question: did your Phytec kit come with two example NK .bin images (NK_ACSY.bin and NK_HOST)? The first one has ActiveSync built into it.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;As for Ethernet, we do not have Ethernet working on our kit yet, I am curious what your Catalog Items settings are for that. &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:28:14 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:28:14Z</dc:date>
    <item>
      <title>How to deploy application to phytec developement board running with NXP WinCE BSP</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-deploy-application-to-phytec-developement-board-running/m-p/544228#M12855</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by joho1997 on Mon Jul 16 05:45:38 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am having problem to connect to the phytec development board. I have built the Win CE image with with KITL disabled and Ethernet Driver selected on the Catalog. I have included the 5 CoreCon files on the image. I have modified the ip address on the platfrom.reg to a fixed ip address. I can download the WinCE image to the target board through ethernet port. I can ping to the target board with the predefined ip address.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have also entered the ip address to Tools-&amp;gt;Options-&amp;gt;Device Tools-&amp;gt;Devices-&amp;gt;Window CE 5.0 Device-&amp;gt;Properties on the VS2005 application instance.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;However, whenever I try to connect to the target device from a VS2005 application instance (a C# application instance), it always reports Connection failed. ActiveSync is not installed.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I watch the packets with WebShark, it shows that the VS2005 application instance sends a request to the target device and the device response to the request. After 3 times of retry, the VS2005 application instance reports the connection error.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Just wonder did anyone successfully deploy application to the Phytec Development Board running the NXP WinCE BSP?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Not sure what I have missed. Can someone please advise.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Many Thanks!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:28:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-deploy-application-to-phytec-developement-board-running/m-p/544228#M12855</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:28:12Z</dc:date>
    </item>
    <item>
      <title>Re: How to deploy application to phytec developement board running with NXP WinCE BSP</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-deploy-application-to-phytec-developement-board-running/m-p/544229#M12856</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by rcsison on Tue Jul 17 14:16:11 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi, we use a Phytec LPC3250 development board. We have used both the NXP WinCE 6.0 BSP for it, as well as one from Adeneo. If I recall (it has been a few months since we tried the NXP BSP, which is a free download), it did not have Active Sync built into it. As for the Adeneo one (which has a free version available as a .bin only without source code), we do have Active Sync running...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You might want to try that BSP on your hardware...&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:28:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-deploy-application-to-phytec-developement-board-running/m-p/544229#M12856</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:28:13Z</dc:date>
    </item>
    <item>
      <title>Re: How to deploy application to phytec developement board running with NXP WinCE BSP</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-deploy-application-to-phytec-developement-board-running/m-p/544230#M12857</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by joho1997 on Wed Jul 18 03:40:08 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi rcsison,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for your advise.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have just downloaded the BSP from Adeneo and built the image, but I am still not able to connect the development board. I can download the Win CE image to the board.&amp;nbsp; With KITL enabled, I can watch the files and the processes.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I built the WinCE image with KITL disable but still not able to connect to the target board. I am sure the core con files (ConmanClient2.exe and CMAccept.exe) are running. I have also include the ActiveSync on the image but no luck.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;How can I find out the IP address for debug connection. I don't have any LCD display connected on the development board (still waiting for delivery).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Do I have install ActiveSync (what version?) and connect with USB for debugger?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is it possible to debug with ethernet connection?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Many Thanks!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:28:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-deploy-application-to-phytec-developement-board-running/m-p/544230#M12857</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:28:14Z</dc:date>
    </item>
    <item>
      <title>Re: How to deploy application to phytec developement board running with NXP WinCE BSP</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-deploy-application-to-phytec-developement-board-running/m-p/544231#M12858</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by rcsison on Wed Jul 18 18:49:35 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;In the Platform Building, we have two things selected in the Catalog Items:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Under Core OS-&amp;gt;Applications - End User, we have "ActiveSync" selected.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Under Third Party-&amp;gt;BSP-&amp;gt;PhyCore_LPC3250: ARMV4I-&amp;gt;USB Drivers, we have "USB Device Driver" selected so ActiveSync will work. "USB Host Driver" is for giving the device the capability to read a USB memory stick.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;A question: did your Phytec kit come with two example NK .bin images (NK_ACSY.bin and NK_HOST)? The first one has ActiveSync built into it.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;As for Ethernet, we do not have Ethernet working on our kit yet, I am curious what your Catalog Items settings are for that. &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:28:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-deploy-application-to-phytec-developement-board-running/m-p/544231#M12858</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:28:14Z</dc:date>
    </item>
    <item>
      <title>Re: How to deploy application to phytec developement board running with NXP WinCE BSP</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-deploy-application-to-phytec-developement-board-running/m-p/544232#M12859</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by joho1997 on Thu Jul 19 06:11:01 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have made a little progress to get the CE image runs with the pre-set IP address (192.168.222.10). However when I try to connect to the target device, it still reports connection failed error.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have captured the log when attempted for the connection (See attached screen dump). It retried for 3 times an then failed.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Wonder what else missing on the settings.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please help!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:28:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-deploy-application-to-phytec-developement-board-running/m-p/544232#M12859</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:28:15Z</dc:date>
    </item>
    <item>
      <title>Re: How to deploy application to phytec developement board running with NXP WinCE BSP</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-deploy-application-to-phytec-developement-board-running/m-p/544233#M12860</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by rcsison on Thu Jul 19 07:58:32 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;joho: Can you please let me know what all your Ethernet-related settings are in the Catalog Items in Platform Builder for both the NXP and Adeneo BSPs? This might help me see what you are seeing...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks...&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:28:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-deploy-application-to-phytec-developement-board-running/m-p/544233#M12860</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:28:16Z</dc:date>
    </item>
    <item>
      <title>Re: How to deploy application to phytec developement board running with NXP WinCE BSP</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-deploy-application-to-phytec-developement-board-running/m-p/544234#M12861</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by joho1997 on Mon Jul 23 04:21:48 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have attached all the screen dump of the CE catalog. I have also modified one of register file to assign a fixed ip address for the OS image.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please advise if I may have missed some settings.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Many Thanks!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:28:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-deploy-application-to-phytec-developement-board-running/m-p/544234#M12861</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:28:16Z</dc:date>
    </item>
  </channel>
</rss>