<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Step Into Function when functions are different memory areas (LPCXPresso IDE) in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Step-Into-Function-when-functions-are-different-memory-areas/m-p/543820#M12769</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Wed Dec 11 07:38:16 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm sorry, but I do not know of any way around this restriction. To step through stubs/veneers you have to single-step the assembler.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;We will raise this issue with the ld maintainers.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:27:19 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:27:19Z</dc:date>
    <item>
      <title>Step Into Function when functions are different memory areas (LPCXPresso IDE)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Step-Into-Function-when-functions-are-different-memory-areas/m-p/543819#M12768</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ajones on Wed Dec 11 05:01:22 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using the LPCXPresso IDE.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have code that is configured to execute from internal SRAM and external SDRAM.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The linker places a __FunctionName_veneer function to handle the large address offset required by the function being in different memory areas.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The debugger won't step into the veneer function when debugging at the C code level - it will do it when I instruction step in the Disassembler Window.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I presume the problem is that the veneer function has no debug information and hence debugger chooses to step over rather than step into.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any ideas on convincing the debugger to perform a step into the function in this situation?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Adrian&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:27:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Step-Into-Function-when-functions-are-different-memory-areas/m-p/543819#M12768</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:27:18Z</dc:date>
    </item>
    <item>
      <title>Re: Step Into Function when functions are different memory areas (LPCXPresso IDE)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Step-Into-Function-when-functions-are-different-memory-areas/m-p/543820#M12769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Wed Dec 11 07:38:16 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm sorry, but I do not know of any way around this restriction. To step through stubs/veneers you have to single-step the assembler.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;We will raise this issue with the ld maintainers.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:27:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Step-Into-Function-when-functions-are-different-memory-areas/m-p/543820#M12769</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:27:19Z</dc:date>
    </item>
  </channel>
</rss>