<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC 3250 I2C transmission issue</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-3250-I2C-transmission-issue/m-p/543717#M12748</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by vikhyathk on Mon Oct 19 22:10:51 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am facing a problem with i2C transmission using LPC3250. I m using processor to interface FPGA with device id 0xA0. So the first data I put into '0x400a8000' (I2C2_TX) register is '0x1A0' and I see in the oscilloscope that start condition is generated and acknowledgement is present. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;But Whenever I send a data byte later&amp;nbsp; with LSB bit '1', the same data is being resent with LSB bit made '0'.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Example: If I put "11011001' into the register '0x400a8000' (I2C2_TX) Data found in scope is ["11011001" 'Ack bit' "11011000"'Ack bit']..&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;'Ack bit' is '0'.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can anybody help me to solve the issue. &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:28:05 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:28:05Z</dc:date>
    <item>
      <title>LPC 3250 I2C transmission issue</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-3250-I2C-transmission-issue/m-p/543717#M12748</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by vikhyathk on Mon Oct 19 22:10:51 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am facing a problem with i2C transmission using LPC3250. I m using processor to interface FPGA with device id 0xA0. So the first data I put into '0x400a8000' (I2C2_TX) register is '0x1A0' and I see in the oscilloscope that start condition is generated and acknowledgement is present. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;But Whenever I send a data byte later&amp;nbsp; with LSB bit '1', the same data is being resent with LSB bit made '0'.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Example: If I put "11011001' into the register '0x400a8000' (I2C2_TX) Data found in scope is ["11011001" 'Ack bit' "11011000"'Ack bit']..&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;'Ack bit' is '0'.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can anybody help me to solve the issue. &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:28:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-3250-I2C-transmission-issue/m-p/543717#M12748</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:28:05Z</dc:date>
    </item>
  </channel>
</rss>