<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC1769 issue with NXP PCF8574P in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-issue-with-NXP-PCF8574P/m-p/543302#M12658</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please can you help me with this? &lt;/P&gt;&lt;P&gt;I´m trying to add 16 additional digital outputs to LCP1769FBD100, using two PCF8574P. For test purposes, I´m using a single PCF &lt;/P&gt;&lt;P&gt;for now. The problem is the PCF doesn´t send the ACK. The curious thing is I´ve tried with 4 different units and one of them worked perfectly&lt;/P&gt;&lt;P&gt;and the rest don´t.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;SPAN style="text-decoration: underline;"&gt;I know it´s not an address issue&lt;/SPAN&gt;. The PCF units are all identical and was tested in the same circuit. For your knowledge, my pullup resistors are &lt;/P&gt;&lt;P&gt;2K2. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is any known issue of incompatibility between these two ICs that can depend of dispersion of the chips or I should assume they sold me three&lt;/P&gt;&lt;P&gt;damaged PCFs? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Aug 2016 16:18:11 GMT</pubDate>
    <dc:creator>fernandoresquín</dc:creator>
    <dc:date>2016-08-19T16:18:11Z</dc:date>
    <item>
      <title>LPC1769 issue with NXP PCF8574P</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-issue-with-NXP-PCF8574P/m-p/543302#M12658</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please can you help me with this? &lt;/P&gt;&lt;P&gt;I´m trying to add 16 additional digital outputs to LCP1769FBD100, using two PCF8574P. For test purposes, I´m using a single PCF &lt;/P&gt;&lt;P&gt;for now. The problem is the PCF doesn´t send the ACK. The curious thing is I´ve tried with 4 different units and one of them worked perfectly&lt;/P&gt;&lt;P&gt;and the rest don´t.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;SPAN style="text-decoration: underline;"&gt;I know it´s not an address issue&lt;/SPAN&gt;. The PCF units are all identical and was tested in the same circuit. For your knowledge, my pullup resistors are &lt;/P&gt;&lt;P&gt;2K2. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is any known issue of incompatibility between these two ICs that can depend of dispersion of the chips or I should assume they sold me three&lt;/P&gt;&lt;P&gt;damaged PCFs? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Aug 2016 16:18:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-issue-with-NXP-PCF8574P/m-p/543302#M12658</guid>
      <dc:creator>fernandoresquín</dc:creator>
      <dc:date>2016-08-19T16:18:11Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1769 issue with NXP PCF8574P</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-issue-with-NXP-PCF8574P/m-p/543303#M12659</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I checked the PCF8574P and LPC1769 errata record, there without related record.&lt;/P&gt;&lt;P&gt;How about the PCF8574P chips' VDD voltage? Is it same with LPC1769 board VDD voltage?&lt;/P&gt;&lt;P&gt;Could you try to change using the 10K pull up resistor instead with 2.2K value?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Sep 2016 02:34:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-issue-with-NXP-PCF8574P/m-p/543303#M12659</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-09-12T02:34:36Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1769 issue with NXP PCF8574P</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-issue-with-NXP-PCF8574P/m-p/543304#M12660</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Hui Ma:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for answering. I really appretiate that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Finally I ´ve solved the issue. I have three of my four PCF8574P that are responding&lt;/P&gt;&lt;P&gt;like they were PCF8574AP, so there were really an addresss problem, but I was not&lt;/P&gt;&lt;P&gt;my mistake. I think these chips are defective or&amp;nbsp;were marked erroneously at the factory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Sep 2016 23:55:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-issue-with-NXP-PCF8574P/m-p/543304#M12660</guid>
      <dc:creator>fernandoresquín</dc:creator>
      <dc:date>2016-09-20T23:55:46Z</dc:date>
    </item>
  </channel>
</rss>