<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Pin state when micro is turned off</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Pin-state-when-micro-is-turned-off/m-p/543145#M12618</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by arw on Tue Dec 30 11:06:53 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If the device is not powered, then the state of the chip is completely undefined.&amp;nbsp; It is dangerous for another device to drive any voltage in a circuit that connects to an IC that is powered off.&amp;nbsp; Either IC may be damaged since the IOs are not in a controlled state.&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If you want to ensure that the device is in a known state, then try using Deep Power-Down mode, for example, which holds all pins (except WAKEUP) in tri-state mode.&amp;nbsp; This will require that you keep an active power supply to the device.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If you must power-off the part of the system where this MCU is included, then all connecting circuits in the powered-on area should be high impedance, and must not drive a voltage on these connecting paths.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;-arw&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:45:40 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:45:40Z</dc:date>
    <item>
      <title>Pin state when micro is turned off</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Pin-state-when-micro-is-turned-off/m-p/543144#M12617</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mattiad on Tue Dec 30 00:40:10 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi everybody,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using an LPCU68 in a particular circuit. In the circuit I use two different supply sources and I turn off the micro in order to go in “power-saving” state (another micro is connected to another suplly and it's always on).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When the LPC is turned off, are all the pins in a not-well-known state? I mean, can some pin be in a high or low logical state with low impedance and draw-source some current?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Is it possible to have all of these in high impedance state?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best regards&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:45:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Pin-state-when-micro-is-turned-off/m-p/543144#M12617</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:45:40Z</dc:date>
    </item>
    <item>
      <title>Re: Pin state when micro is turned off</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Pin-state-when-micro-is-turned-off/m-p/543145#M12618</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by arw on Tue Dec 30 11:06:53 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If the device is not powered, then the state of the chip is completely undefined.&amp;nbsp; It is dangerous for another device to drive any voltage in a circuit that connects to an IC that is powered off.&amp;nbsp; Either IC may be damaged since the IOs are not in a controlled state.&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If you want to ensure that the device is in a known state, then try using Deep Power-Down mode, for example, which holds all pins (except WAKEUP) in tri-state mode.&amp;nbsp; This will require that you keep an active power supply to the device.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If you must power-off the part of the system where this MCU is included, then all connecting circuits in the powered-on area should be high impedance, and must not drive a voltage on these connecting paths.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;-arw&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:45:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Pin-state-when-micro-is-turned-off/m-p/543145#M12618</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:45:40Z</dc:date>
    </item>
  </channel>
</rss>