<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC 1833 Timer</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-1833-Timer/m-p/542968#M12589</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by akshaya.k55 on Wed Oct 14 02:21:59 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a doubt in using timer module of LPC1833 32 bit ARM Cortex M3.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;From the user guide i found like there are four timer modules timers 0/1/2/3 each having 4 channels. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Counter Mode:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to know if I can use all the four channels of all four timer modules at the same time. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;That is, can this be used for 16 different timer inputs simultaneously?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Or only one channel at a time can be active?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have this doubt because there is only one timer counter register present per timer module. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Timer Mode:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Configuring in timer mode, I want to measure 10 different time intervals simultaneously(i.e., starting instant same, ending instant different). Is this possible with the above chip?&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:25:52 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:25:52Z</dc:date>
    <item>
      <title>LPC 1833 Timer</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-1833-Timer/m-p/542968#M12589</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by akshaya.k55 on Wed Oct 14 02:21:59 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a doubt in using timer module of LPC1833 32 bit ARM Cortex M3.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;From the user guide i found like there are four timer modules timers 0/1/2/3 each having 4 channels. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Counter Mode:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to know if I can use all the four channels of all four timer modules at the same time. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;That is, can this be used for 16 different timer inputs simultaneously?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Or only one channel at a time can be active?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have this doubt because there is only one timer counter register present per timer module. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Timer Mode:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Configuring in timer mode, I want to measure 10 different time intervals simultaneously(i.e., starting instant same, ending instant different). Is this possible with the above chip?&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:25:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-1833-Timer/m-p/542968#M12589</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:25:52Z</dc:date>
    </item>
  </channel>
</rss>