<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Where's the loc in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Where-s-the-loc/m-p/542842#M12571</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by IanB on Sat Jan 03 01:58:40 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;On an LPC11xx there are several registers called IOCON_SCK_LOC, IOCON_DSR_LOC etc. which select pin locations.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The LPC11E67 also has movable functions but I see no similar registers. Have I just failed to find them? Are they called something different? or does the 11E67 manage without them.&amp;nbsp; If so, what happens if the same function gets mapped to two different pins in the IOCON registers? (OK you can tell me "Don't do that, it's stupid")&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:44:17 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:44:17Z</dc:date>
    <item>
      <title>Where's the loc</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Where-s-the-loc/m-p/542842#M12571</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by IanB on Sat Jan 03 01:58:40 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;On an LPC11xx there are several registers called IOCON_SCK_LOC, IOCON_DSR_LOC etc. which select pin locations.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The LPC11E67 also has movable functions but I see no similar registers. Have I just failed to find them? Are they called something different? or does the 11E67 manage without them.&amp;nbsp; If so, what happens if the same function gets mapped to two different pins in the IOCON registers? (OK you can tell me "Don't do that, it's stupid")&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:44:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Where-s-the-loc/m-p/542842#M12571</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:44:17Z</dc:date>
    </item>
  </channel>
</rss>