<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic HID USB ROM Driver LPC11U24 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/HID-USB-ROM-Driver-LPC11U24/m-p/542456#M12481</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by tanyashir on Wed Jan 30 12:35:12 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;SPAN&gt;I use HID USB ROM Driver of LPC11U24. I have download examples archive from this link: &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fcontent%2Fnxpfile%2Fsample-code-bundle-lpc11uxx-peripherals-using-lpcxpresso" rel="nofollow" target="_blank"&gt;http://www.lpcware.com/content/nxpfile/sample-code-bundle-lpc11uxx-peripherals-using-lpcxpresso&lt;/A&gt;&lt;SPAN&gt; and I have used example named&amp;nbsp; “USB_ROM_HID” from archive.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This example works. But there is a problem that it sends data with specified intervals. Even if I write zero size of sending bytes to the endpoint, the report goes to the computer, in which the number of bytes is zero.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;How can I do so that data are sending only when I need it? &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:42:01 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:42:01Z</dc:date>
    <item>
      <title>HID USB ROM Driver LPC11U24</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/HID-USB-ROM-Driver-LPC11U24/m-p/542456#M12481</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by tanyashir on Wed Jan 30 12:35:12 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;SPAN&gt;I use HID USB ROM Driver of LPC11U24. I have download examples archive from this link: &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fcontent%2Fnxpfile%2Fsample-code-bundle-lpc11uxx-peripherals-using-lpcxpresso" rel="nofollow" target="_blank"&gt;http://www.lpcware.com/content/nxpfile/sample-code-bundle-lpc11uxx-peripherals-using-lpcxpresso&lt;/A&gt;&lt;SPAN&gt; and I have used example named&amp;nbsp; “USB_ROM_HID” from archive.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This example works. But there is a problem that it sends data with specified intervals. Even if I write zero size of sending bytes to the endpoint, the report goes to the computer, in which the number of bytes is zero.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;How can I do so that data are sending only when I need it? &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:42:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/HID-USB-ROM-Driver-LPC11U24/m-p/542456#M12481</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:42:01Z</dc:date>
    </item>
  </channel>
</rss>