<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 24BIT RGB Signals in Datasheet in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/24BIT-RGB-Signals-in-Datasheet/m-p/515563#M1248</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Wouter on Fri Apr 26 03:01:32 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;Hi Randy,&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Thanks for pointing this out! Indeed it's just a typo, nothing to worry about. I'll submit an UM/DS update request.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;The obvious choices are indeed the right one, so PB_0, PB_1, PB_2, PB_3, P7_1 and P7_2 should be used for BLUE7..BLUE2&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Wouter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:17:04 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:17:04Z</dc:date>
    <item>
      <title>24BIT RGB Signals in Datasheet</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/24BIT-RGB-Signals-in-Datasheet/m-p/515562#M1247</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by RandyM on Thu Apr 25 11:14:26 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;For the LPC435x, on page 131 of the LPC435x datasheet, the LCD panel connection table for TFT seems off. &amp;nbsp;For blue bits [2:7] there are no "pin used" assignments. &amp;nbsp;I'm going to hope that this is a type-o and the obvious choices for pins were just accidently not filled in. &amp;nbsp;Can anyone verify?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:17:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/24BIT-RGB-Signals-in-Datasheet/m-p/515562#M1247</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:17:04Z</dc:date>
    </item>
    <item>
      <title>Re: 24BIT RGB Signals in Datasheet</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/24BIT-RGB-Signals-in-Datasheet/m-p/515563#M1248</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Wouter on Fri Apr 26 03:01:32 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;Hi Randy,&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Thanks for pointing this out! Indeed it's just a typo, nothing to worry about. I'll submit an UM/DS update request.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;The obvious choices are indeed the right one, so PB_0, PB_1, PB_2, PB_3, P7_1 and P7_2 should be used for BLUE7..BLUE2&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Wouter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:17:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/24BIT-RGB-Signals-in-Datasheet/m-p/515563#M1248</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:17:04Z</dc:date>
    </item>
  </channel>
</rss>