<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Pixels problem in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Pixels-problem/m-p/515556#M1245</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by DT1 on Tue Feb 11 14:56:52 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;hum, I found the problem.It was not related to my buffers, but to the SDRAM configuration.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I used a file named SDRAM_Init.c originally taken from an example (can't recall if it was from a Keil example or a LPC one, but it was for the MCB4357 board I'm sure). That configuration was working fine on some MCB4357 boards (that I don't have anymore). After validating that the SDRAM chip had indeed changed between the boards, I used the initialization code made by Keil in the MCB4357 emWin demo and all my problems are gone.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:16:58 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:16:58Z</dc:date>
    <item>
      <title>Pixels problem</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Pixels-problem/m-p/515555#M1244</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by DT1 on Fri Jan 31 14:56:54 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I currently using the MCB4357 dev board. I have a custom application using emWin. When I try to draw something on the screen, some pixels don't behave correctly. The pixels are always the same, but their behavior is not constant.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;For example, let's say I have those pixels that are problematic:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Pixel 1 (located at some x and some y)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Pixel 2 (located at some x and some y)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Pixel 3 (located at some x and some y)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Pixel 4 (located at some x and some y)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;- Execute action 1 (redrawn the whole screen)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Pixels are ok&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Execute action 2 (draw a small bitmap image somewhere in the screen)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Pixel 2 is black instead of white, others are ok.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Execute action 3 (draw a small bitmap image at another place in the screen)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Pixel 2 is ok&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Pixel 1, 3 and 4 are black instead of white.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;etc.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If I redo the above, the same pixels will behave wrongly, but not necessarily in the same order. What I have in mind is a problem with the SDRAM or maybe one of the RGB trace, but my dev board is brand new and I have this problem on another MCB4357 too.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any suggestion on where to look?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:16:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Pixels-problem/m-p/515555#M1244</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:16:57Z</dc:date>
    </item>
    <item>
      <title>Re: Pixels problem</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Pixels-problem/m-p/515556#M1245</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by DT1 on Tue Feb 11 14:56:52 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;hum, I found the problem.It was not related to my buffers, but to the SDRAM configuration.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I used a file named SDRAM_Init.c originally taken from an example (can't recall if it was from a Keil example or a LPC one, but it was for the MCB4357 board I'm sure). That configuration was working fine on some MCB4357 boards (that I don't have anymore). After validating that the SDRAM chip had indeed changed between the boards, I used the initialization code made by Keil in the MCB4357 emWin demo and all my problems are gone.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:16:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Pixels-problem/m-p/515556#M1245</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:16:58Z</dc:date>
    </item>
  </channel>
</rss>