<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Flashing using USB MSC ISP on Linux vs Windows, LPC11U6x in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flashing-using-USB-MSC-ISP-on-Linux-vs-Windows-LPC11U6x/m-p/542228#M12447</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by drs on Fri May 23 14:12:39 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Try skipping the rm command and including the -f flag to the cp command.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:44:19 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:44:19Z</dc:date>
    <item>
      <title>Flashing using USB MSC ISP on Linux vs Windows, LPC11U6x</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flashing-using-USB-MSC-ISP-on-Linux-vs-Windows-LPC11U6x/m-p/542227#M12446</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by acker10 on Sun May 18 07:43:05 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a LPC11U67 where everything seems to be in working order, but I'm observing that if use ISP MSC to copy a firmware file via Windows 7, everything is fine.&amp;nbsp; When I flash the exact same firmware via Linux by doing the following:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;mount /dev/sdd /mnt
rm /mnt/firmware.bin
cp firmware.bin /mnt
sync
umount /mnt&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Then it won't restart into the firmware when I power cycle the MCU.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When I power cycle and remount on Linux, if I look at a hex dump of /mnt/firmware.bin and compare the firmwares copied via Windows with the one copied via Linux, I do notice differences starting at byte location 0x400.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So something about the USB copy transaction is not working the same in Linux as it is in Windows.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Anybody have this working via Linux?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:44:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Flashing-using-USB-MSC-ISP-on-Linux-vs-Windows-LPC11U6x/m-p/542227#M12446</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:44:18Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing using USB MSC ISP on Linux vs Windows, LPC11U6x</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flashing-using-USB-MSC-ISP-on-Linux-vs-Windows-LPC11U6x/m-p/542228#M12447</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by drs on Fri May 23 14:12:39 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Try skipping the rm command and including the -f flag to the cp command.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:44:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Flashing-using-USB-MSC-ISP-on-Linux-vs-Windows-LPC11U6x/m-p/542228#M12447</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:44:19Z</dc:date>
    </item>
  </channel>
</rss>