<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Reset doesn´t work as aspected after Firmwareupdate</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Reset-doesn-t-work-as-aspected-after-Firmwareupdate/m-p/542074#M12416</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mc on Fri Sep 18 11:25:00 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Ben,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It may be going into ISP mode. Could you please ensure that P2_7 is high during boot? You can set this pin in input pull-up mode before invoking core reset. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If something is connected on this pin, please add a pull-up resistor so it is not pull-down by the external component .&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:25:51 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:25:51Z</dc:date>
    <item>
      <title>Reset doesn´t work as aspected after Firmwareupdate</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Reset-doesn-t-work-as-aspected-after-Firmwareupdate/m-p/542072#M12414</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ben Sch on Fri Sep 18 01:28:31 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi there,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;i´m using a LPC1857 and wrote a firmware which uses only one of the internal flash banks. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;After writing a new firmware with the IAP function into the not used flash bank and updating the signatures(old one unvalid, new one valid) i´m trying to do an reset to let the controller start with the internal bootloader to check the signatures and start with the new, valid firmware.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When trying to reset the controller with the CORE reset, it hangs in an unknown state and can only be started again with a hardreset.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If reseting with PERIPHAL or MASTER reset the controller starts the old Firmware with the unvalid signature.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;After a hardreset over the button it starts with the new valid firmware.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can you please help me with a solution to my problem?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks a lot and greetings&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ben&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:25:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Reset-doesn-t-work-as-aspected-after-Firmwareupdate/m-p/542072#M12414</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:25:49Z</dc:date>
    </item>
    <item>
      <title>Re: Reset doesn´t work as aspected after Firmwareupdate</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Reset-doesn-t-work-as-aspected-after-Firmwareupdate/m-p/542073#M12415</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mysepp on Fri Sep 18 10:45:08 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Ben,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;have you seen the errata of LPC1857, especially RGU.1?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Errata can be found here:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.lpcware.com%2Fcontent%2Fnxpfile%2Ferrata-sheet-lpc185x-lpc183x-lpc182x-lpc181x-flash-based-devices-eslpc185x3x2x1xflas" rel="nofollow" target="_blank"&gt;https://www.lpcware.com/content/nxpfile/errata-sheet-lpc185x-lpc183x-lpc182x-lpc181x-flash-based-devices-eslpc185x3x2x1xflas&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Martin&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:25:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Reset-doesn-t-work-as-aspected-after-Firmwareupdate/m-p/542073#M12415</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:25:50Z</dc:date>
    </item>
    <item>
      <title>Re: Reset doesn´t work as aspected after Firmwareupdate</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Reset-doesn-t-work-as-aspected-after-Firmwareupdate/m-p/542074#M12416</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mc on Fri Sep 18 11:25:00 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Ben,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It may be going into ISP mode. Could you please ensure that P2_7 is high during boot? You can set this pin in input pull-up mode before invoking core reset. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If something is connected on this pin, please add a pull-up resistor so it is not pull-down by the external component .&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:25:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Reset-doesn-t-work-as-aspected-after-Firmwareupdate/m-p/542074#M12416</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:25:51Z</dc:date>
    </item>
    <item>
      <title>Re: Reset doesn´t work as aspected after Firmwareupdate</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Reset-doesn-t-work-as-aspected-after-Firmwareupdate/m-p/542075#M12417</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ben Sch on Mon Sep 21 01:31:50 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Martin,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thx, in fact I have the old Revision .4 of the errata, where the RGU is mentioned in the Revision history but then not mentioned in the sheet itself.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This answers the questions about the Master and Peripheral Reset!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thx and greetings&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;ben&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:25:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Reset-doesn-t-work-as-aspected-after-Firmwareupdate/m-p/542075#M12417</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:25:51Z</dc:date>
    </item>
  </channel>
</rss>