<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックAN11175 DALI master bus receive</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/AN11175-DALI-master-bus-receive/m-p/541919#M12384</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by purplexed on Thu Jun 26 06:03:10 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I was analyzing the AN on the subject and I' ve observed a misaligned information between the schematic of the board and the sample code.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In the schematic, DALI bus reception line is connected on TIMER 0 capture 0 and on TIMER 1 match 0, while the code configures and uses timer1 capture and match channels only.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Capture is used to manage the backward frame, but in this case it seems not to care about it because of the improper configuration; so the application works but responses from dali bus appear as always true because the line can't be sampled.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Am I wrong?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:45:27 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:45:27Z</dc:date>
    <item>
      <title>AN11175 DALI master bus receive</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/AN11175-DALI-master-bus-receive/m-p/541919#M12384</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by purplexed on Thu Jun 26 06:03:10 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I was analyzing the AN on the subject and I' ve observed a misaligned information between the schematic of the board and the sample code.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In the schematic, DALI bus reception line is connected on TIMER 0 capture 0 and on TIMER 1 match 0, while the code configures and uses timer1 capture and match channels only.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Capture is used to manage the backward frame, but in this case it seems not to care about it because of the improper configuration; so the application works but responses from dali bus appear as always true because the line can't be sampled.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Am I wrong?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:45:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/AN11175-DALI-master-bus-receive/m-p/541919#M12384</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:45:27Z</dc:date>
    </item>
    <item>
      <title>Re: AN11175 DALI master bus receive</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/AN11175-DALI-master-bus-receive/m-p/541920#M12385</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Irving on Tue Aug 05 00:14:40 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi purplexed,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It's a good question, and you analyzd very carefully. Actually, we didn't use timer1 match0 function, but we use PIO1_1 as GPIO. The timer0 capture0 is used as capture the DALI bus Rx pin timer count between rising and failing edges. And PIO1_1 is used as GPIO to read DALI bus Rx pin level (Low/High). Thank you.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:45:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/AN11175-DALI-master-bus-receive/m-p/541920#M12385</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:45:28Z</dc:date>
    </item>
  </channel>
</rss>