<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Need help with LPC11xx in own application!</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Need-help-with-LPC11xx-in-own-application/m-p/541876#M12376</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by R2D2 on Tue May 20 03:39:03 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Since VBE of BC847 is 0.7V this 100k resistor is not the worst problem...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Anyway, to avoid problems it's a good idea to use active low switching with P-Channel FET (BSS84) ...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;SPAN&gt;See: &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Famateurfunkbasteln.de%2Fmosfets_und_co%2Findex.html" rel="nofollow" target="_blank"&gt;http://amateurfunkbasteln.de/mosfets_und_co/index.html&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So default GPIO setup (input &amp;amp; pull-up) doesn't cause unintended behavior...&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:43:41 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:43:41Z</dc:date>
    <item>
      <title>Need help with LPC11xx in own application!</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Need-help-with-LPC11xx-in-own-application/m-p/541870#M12370</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Martin84 on Mon May 19 13:59:24 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm trying to use the LPC1113/301 and LPC1114/301 in my own application. The LPC1113 is soldered on an own application board. Because I have a problem with programming the LPC1113 I have also tried to integrate the LPCXpresso Board with the LPC1114 in my own application. In both cases I can't program the LPC with "Debug" command. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If I directly use the "Program flash" command everything works fine. In another thread I read that other users had success with disabling Interrupts. Where can I do this?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;After completion of programming the .axf to flash, I get the message "Executing in bootloader". &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Now when I'm trying the same with the LPC1769 Xpresso Board I can use the "Debug" command without any problems. And when I'm using the "Program flash" command, I get the message "executing in user flash". &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What do I have to configure for the LPC111x µCs and where can I do this?&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:43:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Need-help-with-LPC11xx-in-own-application/m-p/541870#M12370</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:43:37Z</dc:date>
    </item>
    <item>
      <title>Re: Need help with LPC11xx in own application!</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Need-help-with-LPC11xx-in-own-application/m-p/541871#M12371</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by R2D2 on Mon May 19 14:30:59 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt; :quest: &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Without knowing your hardware and without knowing your project, there's not much help to offer...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Usually LPC11xx are working without problems&amp;nbsp;&amp;nbsp; :)&amp;nbsp;&amp;nbsp; if you don't violate basic rules: &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fcontent%2Ffaq%2Flpcxpresso%2Fregaining-debug-access" rel="nofollow" target="_blank"&gt;http://www.lpcware.com/content/faq/lpcxpresso/regaining-debug-access&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Anyway, after booting into ISP flashing and debugging a simple sample program should always be possible.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If that's not possible it's useful to check your hardware...&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:43:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Need-help-with-LPC11xx-in-own-application/m-p/541871#M12371</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:43:38Z</dc:date>
    </item>
    <item>
      <title>Re: Need help with LPC11xx in own application!</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Need-help-with-LPC11xx-in-own-application/m-p/541872#M12372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Martin84 on Tue May 20 00:37:27 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks for your reply R2D2. I use the GPIOs for switching BC847 transistors. As I tried my hardware with a simple program code I used the P0.1 Pin. Now I read that P0.1 is the ISP-Pin for the LPC11xx. Could it be the problem that I switched the ISP-Pin and set the LPC in reset while programming in SWD Mode?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;That could be an explanation for the problem on both Controllers (the LPC1113 on own PCB and the LPCXpresso LPC1114). So I will try to regain the debug access with your link :-)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there anybody who has had the same problem? &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards, &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Martin &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:43:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Need-help-with-LPC11xx-in-own-application/m-p/541872#M12372</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:43:38Z</dc:date>
    </item>
    <item>
      <title>Re: Need help with LPC11xx in own application!</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Need-help-with-LPC11xx-in-own-application/m-p/541873#M12373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by starblue on Tue May 20 00:56:15 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: Martin84&lt;/STRONG&gt;&lt;BR /&gt;I use the GPIOs for switching BC847 transistors.&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Probably the transistor is pulling the pin low?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:43:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Need-help-with-LPC11xx-in-own-application/m-p/541873#M12373</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:43:39Z</dc:date>
    </item>
    <item>
      <title>Re: Need help with LPC11xx in own application!</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Need-help-with-LPC11xx-in-own-application/m-p/541874#M12374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by R2D2 on Tue May 20 01:36:51 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: Martin84&lt;/STRONG&gt;&lt;BR /&gt;Is there anybody who has had the same problem? &lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Yes, that's an usual error&amp;nbsp; :) &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fcontent%2Fforum%2Fp210-as-gpio-not-working" rel="nofollow" target="_blank"&gt;http://www.lpcware.com/content/forum/p210-as-gpio-not-working&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If it's possible, just avoid to use ISP pins (at least as output).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;A P-Channel FET like BSS84P (LOW active) is a better solution than a pnp BJT... &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;But anyway, a strong pull-up will solve your ISP problem...&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:43:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Need-help-with-LPC11xx-in-own-application/m-p/541874#M12374</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:43:40Z</dc:date>
    </item>
    <item>
      <title>Re: Need help with LPC11xx in own application!</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Need-help-with-LPC11xx-in-own-application/m-p/541875#M12375</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Martin84 on Tue May 20 02:35:27 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;I am using LPC1769. I configured pin P2.10 as GPIO, but when board is connected to the application, code is running strangely and debugging is not possible. When I disconnected pin P2.10 only, everything works fine. I tried repeat connection/disconnection of P2.10 and still with same result (connected=NOK, disconnected=OK). Do you know what can be the reason of such behavior? Pin P2.10 is physically connected to base of the bipolar NPN transistor.&lt;BR /&gt;Thank you.&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;That's exactly the same Problem.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In the attachment there is the problem shown...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I will try it when I'm home. I think I will avoid using the P0.1.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you very much for the great answer :-) I will report the results of this solution!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards, Martin &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:43:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Need-help-with-LPC11xx-in-own-application/m-p/541875#M12375</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:43:40Z</dc:date>
    </item>
    <item>
      <title>Re: Need help with LPC11xx in own application!</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Need-help-with-LPC11xx-in-own-application/m-p/541876#M12376</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by R2D2 on Tue May 20 03:39:03 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Since VBE of BC847 is 0.7V this 100k resistor is not the worst problem...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Anyway, to avoid problems it's a good idea to use active low switching with P-Channel FET (BSS84) ...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;SPAN&gt;See: &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Famateurfunkbasteln.de%2Fmosfets_und_co%2Findex.html" rel="nofollow" target="_blank"&gt;http://amateurfunkbasteln.de/mosfets_und_co/index.html&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So default GPIO setup (input &amp;amp; pull-up) doesn't cause unintended behavior...&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:43:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Need-help-with-LPC11xx-in-own-application/m-p/541876#M12376</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:43:41Z</dc:date>
    </item>
    <item>
      <title>Re: Need help with LPC11xx in own application!</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Need-help-with-LPC11xx-in-own-application/m-p/541877#M12377</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MarcVonWindscooting on Tue May 20 12:22:36 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;If you insist on bipolar junction transistors, you should use emitter-follower configurations for high(er) input impedance. Probably without a base resistor to avoid excessive voltage drop.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:43:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Need-help-with-LPC11xx-in-own-application/m-p/541877#M12377</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:43:42Z</dc:date>
    </item>
    <item>
      <title>Re: Need help with LPC11xx in own application!</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Need-help-with-LPC11xx-in-own-application/m-p/541878#M12378</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Martin84 on Tue May 20 15:07:24 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hey :-)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;now everything is working fine!! I can use the "Debug" command and everything is alright :-) I just avoid using P0.1 and there should be no problem :-) &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;THANK YOU VERY MUCH for the help!!! :-)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This works also for the LPC1113 on my own PCB :-) &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:43:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Need-help-with-LPC11xx-in-own-application/m-p/541878#M12378</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:43:43Z</dc:date>
    </item>
  </channel>
</rss>