<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックMemory in Framebuffer with 18-bit per Pixel</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Memory-in-Framebuffer-with-18-bit-per-Pixel/m-p/515530#M1234</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Martin84 on Wed Jul 31 00:40:38 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using an 18-bit TFT and I wanna calculate the memory that one frame will need. The resolution is 640x480, so I calculate as follows: 640*480*18bit = 5529600 bits -&amp;gt; 5529600 / 8 = 691200 Bytes = 691kB. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is the calculation with 18-bit correct or do i have to use 32-bit?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Martin &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:18:35 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:18:35Z</dc:date>
    <item>
      <title>Memory in Framebuffer with 18-bit per Pixel</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Memory-in-Framebuffer-with-18-bit-per-Pixel/m-p/515530#M1234</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Martin84 on Wed Jul 31 00:40:38 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using an 18-bit TFT and I wanna calculate the memory that one frame will need. The resolution is 640x480, so I calculate as follows: 640*480*18bit = 5529600 bits -&amp;gt; 5529600 / 8 = 691200 Bytes = 691kB. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is the calculation with 18-bit correct or do i have to use 32-bit?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Martin &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:18:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Memory-in-Framebuffer-with-18-bit-per-Pixel/m-p/515530#M1234</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:18:35Z</dc:date>
    </item>
    <item>
      <title>Re: Memory in Framebuffer with 18-bit per Pixel</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Memory-in-Framebuffer-with-18-bit-per-Pixel/m-p/515531#M1235</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Wouter on Wed Jul 31 01:01:37 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Martin,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You would need to use 32bpp framebuffer for 18-bit RGB.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I'd recommend to switch to 5:6:5 (16-bit) mode. This will save memory, but more importantly reduce the bus bandwidth used by the LCD controller.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;You can wire your display for 18-bit mode, and always decide in SW to use 16-bit or 18-bit mode.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Wouter&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:18:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Memory-in-Framebuffer-with-18-bit-per-Pixel/m-p/515531#M1235</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:18:36Z</dc:date>
    </item>
    <item>
      <title>Re: Memory in Framebuffer with 18-bit per Pixel</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Memory-in-Framebuffer-with-18-bit-per-Pixel/m-p/515532#M1236</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Martin84 on Wed Jul 31 02:58:48 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Ok thank you :-)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Martin&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:18:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Memory-in-Framebuffer-with-18-bit-per-Pixel/m-p/515532#M1236</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:18:36Z</dc:date>
    </item>
  </channel>
</rss>