<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC1837 USART in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1837-USART/m-p/541017#M12193</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by taz9557 on Wed Apr 02 13:22:29 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I’m using LPC1837 running at 180MHz in my project, I need to use USART2,3 as high speed half duplex RS485 (baud rate = 6Mbits). I’ve configured my hardware and got it running up to 3Mbits without any problem but any speed above this receives incorrect characters in without any framing errors. i.e. if I transmit 0x55 I receive 0x5B. Has anyone come across this problem or has anyone got a suggestion.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Your help be most appreciated. Thanks&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:23:54 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:23:54Z</dc:date>
    <item>
      <title>LPC1837 USART</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1837-USART/m-p/541017#M12193</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by taz9557 on Wed Apr 02 13:22:29 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I’m using LPC1837 running at 180MHz in my project, I need to use USART2,3 as high speed half duplex RS485 (baud rate = 6Mbits). I’ve configured my hardware and got it running up to 3Mbits without any problem but any speed above this receives incorrect characters in without any framing errors. i.e. if I transmit 0x55 I receive 0x5B. Has anyone come across this problem or has anyone got a suggestion.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Your help be most appreciated. Thanks&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:23:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1837-USART/m-p/541017#M12193</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:23:54Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1837 USART</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1837-USART/m-p/541018#M12194</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by xianghuiwang on Thu Apr 17 17:08:08 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi, taz9557,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can you check is you run into the following limitation?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If the fractional divider is active (DIVADDVAL &amp;gt; 0) and DLM = 0, the value of the DLL register must be 3 or greater.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This is a direction quote from the user manual.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In general, over 3Mbits is no problem, but no all the desired rates are available.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:23:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1837-USART/m-p/541018#M12194</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:23:55Z</dc:date>
    </item>
  </channel>
</rss>