<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Negative ADC voltage affecting other ADC channels in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Negative-ADC-voltage-affecting-other-ADC-channels/m-p/540942#M12171</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by VigneshEP on Mon Aug 25 04:14:44 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm facing a peculiar issue. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[list=1]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]In my application, channel AD2 (PIO1.1) is driven by a source with 50 kOhms impedance. It will always see a voltage between 0 and 3V3&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]AD6 (PIO1.10) can get negative voltage, but not negative than a diode drop below 0 V. This is driven by an impedance of 2 kOhms&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]While AD6 sees -100 mV (negative 100 mV), measurement of AD2 is affected probably by same amount&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/list]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I could see the voltage on AD2 going low whenever AD6 is seeing a negative voltage. If I set A/D bit of IOCON of PIO1.10 as digital (so that analog mux is decoupled from the pin), then there is no 'cross talk'. I haven't checked whether the cross talk exists between any other channel.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Has anyone observed this? It is not mentioned in errata as well. I'm using LPC1114FBD48/323.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Vignesh&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:40:36 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:40:36Z</dc:date>
    <item>
      <title>Negative ADC voltage affecting other ADC channels</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Negative-ADC-voltage-affecting-other-ADC-channels/m-p/540942#M12171</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by VigneshEP on Mon Aug 25 04:14:44 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm facing a peculiar issue. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[list=1]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]In my application, channel AD2 (PIO1.1) is driven by a source with 50 kOhms impedance. It will always see a voltage between 0 and 3V3&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]AD6 (PIO1.10) can get negative voltage, but not negative than a diode drop below 0 V. This is driven by an impedance of 2 kOhms&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]While AD6 sees -100 mV (negative 100 mV), measurement of AD2 is affected probably by same amount&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/list]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I could see the voltage on AD2 going low whenever AD6 is seeing a negative voltage. If I set A/D bit of IOCON of PIO1.10 as digital (so that analog mux is decoupled from the pin), then there is no 'cross talk'. I haven't checked whether the cross talk exists between any other channel.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Has anyone observed this? It is not mentioned in errata as well. I'm using LPC1114FBD48/323.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Vignesh&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:40:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Negative-ADC-voltage-affecting-other-ADC-channels/m-p/540942#M12171</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:40:36Z</dc:date>
    </item>
  </channel>
</rss>