<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: The spec clarifying for LPC185x. in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/The-spec-clarifying-for-LPC185x/m-p/540858#M12151</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by starblue on Tue Sep 01 05:10:17 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;For electrical characteristics like drive strengths, take a look at the data sheet.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:27:11 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:27:11Z</dc:date>
    <item>
      <title>The spec clarifying for LPC185x.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/The-spec-clarifying-for-LPC185x/m-p/540857#M12150</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CH Wu on Sun Aug 30 18:44:23 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello NXP team,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have few questions regarding the spec description of LPC185x.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I want NXP member feedback me these questions because that are very important to us.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1.There are many descriptions in the user manual as following but didn’t descript the “O”. What is the “O” meaning for reset state of GPIO?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[1] N = neutral, input buffer disabled; no extra VDDIO current consumption if the input is driven midway between supplies; set the EZI bit in the SFS register to enable the input buffer; I = input; OL = output driving LOW; OH = output driving HIGH; AI/O = analog input/output; IA= inactive; PU = pull-up enabled (weak pull-up resistor pulls up pin to VDDIO; F = floating. Reset state reflects the pin state at reset without boot code operation.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2.The reset state was descripted in user manual for GPIO status indication. Does the “Reset state” mean the reset pin keeping at low?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3.What is the meaning for normal drive strength &amp;amp; high drive strength?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I captured the following description from UM10430 for question 3.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[2] 5 V tolerant pad with 15 ns glitch filter (5 V tolerant if VDDIO present; if VDDIO not present, do not exceed 3.6 V); provides digital I/O functions with TTL levels and hysteresis; normal drive strength.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[3] 5 V tolerant pad with 15 ns glitch filter (5 V tolerant if VDDIO present; if VDDIO not present, do not exceed 3.6 V); provides digital I/O functions with TTL levels, and hysteresis; high drive strength.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;4.The P3_2 is “OL” during “Reset state” descripted in UM10430. What are the configurations of I/O pas? I referred to the block diagram of the I/O pad but I can’t figure out the configurations.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Please refer to the Fig. 34. Block diagram of the I/O pad of UM10430.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:27:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/The-spec-clarifying-for-LPC185x/m-p/540857#M12150</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:27:10Z</dc:date>
    </item>
    <item>
      <title>Re: The spec clarifying for LPC185x.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/The-spec-clarifying-for-LPC185x/m-p/540858#M12151</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by starblue on Tue Sep 01 05:10:17 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;For electrical characteristics like drive strengths, take a look at the data sheet.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:27:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/The-spec-clarifying-for-LPC185x/m-p/540858#M12151</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:27:11Z</dc:date>
    </item>
  </channel>
</rss>