<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックGPIO interrupt delay on LPC 1769</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/GPIO-interrupt-delay-on-LPC-1769/m-p/539781#M11937</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everybody,&lt;/P&gt;&lt;P&gt;I'm new here and I have a small problem with the GPIO interrupt ( LPC 1769). I manage to run the "Pinint.c" program, both with rising or falling edge. But i would like to know if it's normal to have a constant 1.5 micro second delay between the edge of my signal and the start of the handler. I just switch on a led in the interruption program and i can see that the led is on 1.5 microsecond after the edge of my signal.&lt;/P&gt;&lt;P&gt;It seems long and i would like to decrease that but it's like it cannot be shortened. What is the reason of that delay? I read that this GPIO is asynchronous so it should be shorter that a microsecond, isn't it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for my english, hoping i'm understandable!&lt;/P&gt;&lt;P&gt;Romain&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 09:45:00 GMT</pubDate>
    <dc:creator>romainhuet</dc:creator>
    <dc:date>2016-06-16T09:45:00Z</dc:date>
    <item>
      <title>GPIO interrupt delay on LPC 1769</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/GPIO-interrupt-delay-on-LPC-1769/m-p/539781#M11937</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everybody,&lt;/P&gt;&lt;P&gt;I'm new here and I have a small problem with the GPIO interrupt ( LPC 1769). I manage to run the "Pinint.c" program, both with rising or falling edge. But i would like to know if it's normal to have a constant 1.5 micro second delay between the edge of my signal and the start of the handler. I just switch on a led in the interruption program and i can see that the led is on 1.5 microsecond after the edge of my signal.&lt;/P&gt;&lt;P&gt;It seems long and i would like to decrease that but it's like it cannot be shortened. What is the reason of that delay? I read that this GPIO is asynchronous so it should be shorter that a microsecond, isn't it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for my english, hoping i'm understandable!&lt;/P&gt;&lt;P&gt;Romain&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 09:45:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/GPIO-interrupt-delay-on-LPC-1769/m-p/539781#M11937</guid>
      <dc:creator>romainhuet</dc:creator>
      <dc:date>2016-06-16T09:45:00Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO interrupt delay on LPC 1769</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/GPIO-interrupt-delay-on-LPC-1769/m-p/539782#M11938</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;bump&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Jun 2016 01:13:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/GPIO-interrupt-delay-on-LPC-1769/m-p/539782#M11938</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-19T01:13:20Z</dc:date>
    </item>
  </channel>
</rss>