<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC11C14 - problems during the switch on phase in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11C14-problems-during-the-switch-on-phase/m-p/539702#M11926</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mattiad on Thu Oct 16 05:40:36 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi everyone,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm having some problems during the switching on phase of a LPC11C14 microprocessor.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In my context I supply the micro with 3.3V but I have a supply voltage that has a long rise time (caused by the kind of supplying devices). &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;RESET pin is connected in a "classical" way in a RC filter which is connected to the supply voltage (see the picture attached).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Sometimes the delay caused by the RC is not enough and the micro exits from the reset mode too early and the micro results totally blocked.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;To solve this problem without an hardware modification I wolud like to put an additional delay in the reset port, for example of 200/300 ms.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I mean: if the reset port sense the logic state 1, it give the command to exit from the reset only 300 ms later.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you in advance,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Mattia&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:39:37 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:39:37Z</dc:date>
    <item>
      <title>LPC11C14 - problems during the switch on phase</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11C14-problems-during-the-switch-on-phase/m-p/539702#M11926</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mattiad on Thu Oct 16 05:40:36 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi everyone,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm having some problems during the switching on phase of a LPC11C14 microprocessor.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In my context I supply the micro with 3.3V but I have a supply voltage that has a long rise time (caused by the kind of supplying devices). &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;RESET pin is connected in a "classical" way in a RC filter which is connected to the supply voltage (see the picture attached).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Sometimes the delay caused by the RC is not enough and the micro exits from the reset mode too early and the micro results totally blocked.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;To solve this problem without an hardware modification I wolud like to put an additional delay in the reset port, for example of 200/300 ms.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I mean: if the reset port sense the logic state 1, it give the command to exit from the reset only 300 ms later.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you in advance,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Mattia&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:39:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11C14-problems-during-the-switch-on-phase/m-p/539702#M11926</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:39:37Z</dc:date>
    </item>
  </channel>
</rss>