<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: OV7670 interfacing with LPC1857 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/OV7670-interfacing-with-LPC1857/m-p/538436#M11679</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by bavarian on Tue Apr 19 01:17:18 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The error is created from the linker, which sees more memory allocation in your code than it has available according to the given linker script file.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I don't expect that the freertos_blinky example sets up the external SDRAM, but the camera example requires for sure more RAM than a blinky example.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;A camera module with VGA and RGB565 mode requires 640*480*16bits = 614.400bytes per frame buffer.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This for sure does not fit into the internal SRAM which is limited to 136kbyte.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So please add code which sets up the SDRAM, then you can hard code the frame buffer address to this memory.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Alternatively look for an example which uses the SDRAM anyway and put the camera example mode into that.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;NXP Support Team&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:22:30 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:22:30Z</dc:date>
    <item>
      <title>OV7670 interfacing with LPC1857</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/OV7670-interfacing-with-LPC1857/m-p/538435#M11678</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by dhaval.chauhan on Tue Apr 12 05:43:00 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have MCB1857 development board and OV7670 camera module.I want to display image taken by camera module in Display of development board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have used source code "SCTCameraInterface_software_lpc1857" given on NXP website.When i programmed binary produced in Keil for this project , it is not working.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So i took source code of camera and merged it with "freertos_blinky" example code.Here i have used main function of Camera code as one thread.I am getting following error:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-------------------------------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Finished building: ../example/src/SCTCamDemo.c&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Building target: freertos_blinky.axf&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Invoking: MCU Linker&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;arm-none-eabi-gcc -nostdlib -L"C:\NXP\workspace\lpc_chip_18xx\Debug" -L"C:\NXP\workspace\lpc_board_keil_mcb_1857\Debug" -Xlinker -Map="freertos_blinky.map" -Xlinker --gc-sections -mcpu=cortex-m3 -mthumb -T "freertos_blinky_Debug.ld" -L C:\NXP\workspace\freertos_blinky\Debug -o "freertos_blinky.axf"&amp;nbsp; ./freertos/src/FreeRTOSCommonHooks.o ./freertos/src/croutine.o ./freertos/src/event_groups.o ./freertos/src/heap_3.o ./freertos/src/list.o ./freertos/src/port.o ./freertos/src/queue.o ./freertos/src/tasks.o ./freertos/src/timers.o&amp;nbsp; ./example/src/Cam_OV7670.o ./example/src/FraBufQ.o ./example/src/GLCD_LPC18xx.o ./example/src/I2CRegIO.o ./example/src/LCDRfrsh_MCB1800.o ./example/src/SCTCamDemo.o ./example/src/core_cm3.o ./example/src/cr_startup_lpc18xx.o ./example/src/freertos_blinky.o ./example/src/jtag_dbg_printf.o ./example/src/lpc18xx_cgu.o ./example/src/lpc18xx_i2c.o ./example/src/lpc18xx_scu.o ./example/src/sysinit.o&amp;nbsp;&amp;nbsp; -llpc_board_keil_mcb_1857 -llpc_chip_18xx&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;c:/nxp/lpcxpresso_8.0.0_526/lpcxpresso/tools/bin/../lib/gcc/arm-none-eabi/4.9.3/../../../../arm-none-eabi/bin/ld.exe: freertos_blinky.axf section `SECT_SDRAMRAW' will not fit in region `RamLoc32'&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;c:/nxp/lpcxpresso_8.0.0_526/lpcxpresso/tools/bin/../lib/gcc/arm-none-eabi/4.9.3/../../../../arm-none-eabi/bin/ld.exe: region `RamLoc32' overflowed by 583760 bytes&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;collect2.exe: error: ld returned 1 exit status&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;make: *** [freertos_blinky.axf] Error 1&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-----------------------------------------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;How to solve this issue of Ram overflow?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Dhaval&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:22:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/OV7670-interfacing-with-LPC1857/m-p/538435#M11678</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:22:29Z</dc:date>
    </item>
    <item>
      <title>Re: OV7670 interfacing with LPC1857</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/OV7670-interfacing-with-LPC1857/m-p/538436#M11679</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by bavarian on Tue Apr 19 01:17:18 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The error is created from the linker, which sees more memory allocation in your code than it has available according to the given linker script file.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I don't expect that the freertos_blinky example sets up the external SDRAM, but the camera example requires for sure more RAM than a blinky example.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;A camera module with VGA and RGB565 mode requires 640*480*16bits = 614.400bytes per frame buffer.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This for sure does not fit into the internal SRAM which is limited to 136kbyte.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So please add code which sets up the SDRAM, then you can hard code the frame buffer address to this memory.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Alternatively look for an example which uses the SDRAM anyway and put the camera example mode into that.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;NXP Support Team&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:22:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/OV7670-interfacing-with-LPC1857/m-p/538436#M11679</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:22:30Z</dc:date>
    </item>
    <item>
      <title>Re: OV7670 interfacing with LPC1857</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/OV7670-interfacing-with-LPC1857/m-p/538437#M11680</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;bump&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Jun 2016 01:07:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/OV7670-interfacing-with-LPC1857/m-p/538437#M11680</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-19T01:07:58Z</dc:date>
    </item>
  </channel>
</rss>