<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 hwCAN_MsgTransmit fail with bit0error</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/hwCAN-MsgTransmit-fail-with-bit0error/m-p/538235#M11636</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi, &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Im using the sample "ccan_rom" from the lpcopn 2.20 with my own hardware platform.&lt;/P&gt;&lt;P&gt;The CAN high and low are located on pin 13 and 18. TJA1051 used.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But when I call the hwCAN_MsgTransmit i get an Bit0Error? I can't even moved the TD/RD pins in test mode?&lt;/P&gt;&lt;P&gt;The TJA1051 is connected correct..&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any idea's?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 Jul 2016 08:37:18 GMT</pubDate>
    <dc:creator>thomasjohansen</dc:creator>
    <dc:date>2016-07-05T08:37:18Z</dc:date>
    <item>
      <title>hwCAN_MsgTransmit fail with bit0error</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/hwCAN-MsgTransmit-fail-with-bit0error/m-p/538235#M11636</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi, &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Im using the sample "ccan_rom" from the lpcopn 2.20 with my own hardware platform.&lt;/P&gt;&lt;P&gt;The CAN high and low are located on pin 13 and 18. TJA1051 used.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But when I call the hwCAN_MsgTransmit i get an Bit0Error? I can't even moved the TD/RD pins in test mode?&lt;/P&gt;&lt;P&gt;The TJA1051 is connected correct..&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any idea's?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jul 2016 08:37:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/hwCAN-MsgTransmit-fail-with-bit0error/m-p/538235#M11636</guid>
      <dc:creator>thomasjohansen</dc:creator>
      <dc:date>2016-07-05T08:37:18Z</dc:date>
    </item>
    <item>
      <title>Re: hwCAN_MsgTransmit fail with bit0error</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/hwCAN-MsgTransmit-fail-with-bit0error/m-p/538236#M11637</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Thomas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you tell us which LPC MCU are you using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Carlos Mendoza&lt;/P&gt;&lt;P&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jul 2016 21:10:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/hwCAN-MsgTransmit-fail-with-bit0error/m-p/538236#M11637</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2016-07-14T21:10:18Z</dc:date>
    </item>
  </channel>
</rss>