<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SSP using Keil/NXP SSP Example in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/SSP-using-Keil-NXP-SSP-Example/m-p/537505#M11472</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by John@MPL on Tue Jan 28 09:45:04 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Re: SSP Sample Code on LPC11Axx&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have loaded sample code for the SSP onto a LPC11A14FHN33/301&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have configured the code in loopback mode and linked MISO-1 and MOSI-1&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I cannot appear to get any clocks from SClk after Reset.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Some of the GPIO set up does not apply to the 33 pin device.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am unclear on the SSEL signal and the use.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I would be grateful for any information on the set up.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;John W.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:38:09 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:38:09Z</dc:date>
    <item>
      <title>SSP using Keil/NXP SSP Example</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SSP-using-Keil-NXP-SSP-Example/m-p/537505#M11472</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by John@MPL on Tue Jan 28 09:45:04 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Re: SSP Sample Code on LPC11Axx&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have loaded sample code for the SSP onto a LPC11A14FHN33/301&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have configured the code in loopback mode and linked MISO-1 and MOSI-1&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I cannot appear to get any clocks from SClk after Reset.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Some of the GPIO set up does not apply to the 33 pin device.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am unclear on the SSEL signal and the use.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I would be grateful for any information on the set up.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;John W.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:38:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SSP-using-Keil-NXP-SSP-Example/m-p/537505#M11472</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:38:09Z</dc:date>
    </item>
    <item>
      <title>Re: SSP using Keil/NXP SSP Example</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SSP-using-Keil-NXP-SSP-Example/m-p/537506#M11473</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by John@MPL on Fri Jan 31 02:20:21 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Re Sample Code.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have replaced the LPC14Axx and the SPI now works OK.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;John W&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:38:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SSP-using-Keil-NXP-SSP-Example/m-p/537506#M11473</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:38:10Z</dc:date>
    </item>
    <item>
      <title>Re: SSP using Keil/NXP SSP Example</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SSP-using-Keil-NXP-SSP-Example/m-p/537507#M11474</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by John@MPL on Sat Feb 08 10:36:58 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Re:- LPC11A14 33 pin.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have set up the Demo code for using loopback and works OK if I increment say dest_addr[x] an error occures.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have switched to TX_RX_ONLY&amp;nbsp; = 1 and USE_CS = 1. and using SSP_NUM = 1&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In SSP_Init I have set&amp;nbsp; LPC_SSP1-&amp;gt;CR0 = 0x070f;&amp;nbsp;&amp;nbsp;&amp;nbsp; // 16 bit transfer and changed all 8bit refences to 16bit&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I can send data to a DAC OK but&amp;nbsp; cannot receive from SPI device.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I can see the CS_ toggle and load data out to the MISO Input.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In MAIN my code is:-&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIOSetBitValue( PORT0, 4, 1 ); // Enable Gate to SPI device&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; for ( x = 0; x &amp;lt; 100; x++ );// Allow to settle&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; SSP_Receive( SSP_NUM, (uint16_t *)dest_addr16, 1 );&amp;nbsp; // Set one word into buffer&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; for ( x = 0; x &amp;lt; 100; x++ );// Short delay&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt; GPIOSetBitValue( PORT0, 4, 0 ); // Disable Gate to SPI Device&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt; src_addr16[0] = dest_addr16[0];&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Put received data into src_addr16 to send to DAC&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // if I do scr_addr16[0]&amp;nbsp; =&amp;nbsp; 0x1800;&amp;nbsp;&amp;nbsp; // DAC and has correct value with a range from 0x0000 to 0x3fff&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt; GPIOSetBitValue( PORT0, 26, 1 ); // Enable DAC Output&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt; SSP_Send( SSP_NUM, (uint16_t *)src_addr16, 1);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt; GPIOSetBitValue( PORT0, 26, 0 ); // Disable DAC Output&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I do not appear to get the correct value from dest_addr16[0] &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The SSP_Send and Receives are as is.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any help would be appreciated.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;regards John W.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:38:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SSP-using-Keil-NXP-SSP-Example/m-p/537507#M11474</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:38:10Z</dc:date>
    </item>
  </channel>
</rss>