<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC1857 Flash Issues</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1857-Flash-Issues/m-p/537465#M11461</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by dsidlauskas on Thu Jun 19 12:47:25 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a project that puts all code in Flash Bank A, so that Bank A has a valid code signature. I have a constant data structure located at the beginning of BANK B. When I inadvertently set the first 8 words of this structure to 0, the program stopped loading correctly at startup. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Fig. 10 and Section 4.3.1 of the LPC1857 manual states the if Bank A contains a valid signature, then Bank A will be taken as the boot loader image regardless of the signature in Bank B. My experience suggests that this is not the case.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using Keil Uv4. When the first 8 words in bank B are 0, the debugger starts with the PC and SP at zero. When they're non-zero the PC and SP are set correctly to run the code in Bank A.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does anyone have any comments on what's going on?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Dave&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:20:59 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:20:59Z</dc:date>
    <item>
      <title>LPC1857 Flash Issues</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1857-Flash-Issues/m-p/537465#M11461</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by dsidlauskas on Thu Jun 19 12:47:25 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a project that puts all code in Flash Bank A, so that Bank A has a valid code signature. I have a constant data structure located at the beginning of BANK B. When I inadvertently set the first 8 words of this structure to 0, the program stopped loading correctly at startup. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Fig. 10 and Section 4.3.1 of the LPC1857 manual states the if Bank A contains a valid signature, then Bank A will be taken as the boot loader image regardless of the signature in Bank B. My experience suggests that this is not the case.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using Keil Uv4. When the first 8 words in bank B are 0, the debugger starts with the PC and SP at zero. When they're non-zero the PC and SP are set correctly to run the code in Bank A.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does anyone have any comments on what's going on?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Dave&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:20:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1857-Flash-Issues/m-p/537465#M11461</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:20:59Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1857 Flash Issues</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1857-Flash-Issues/m-p/537466#M11462</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by bavarian on Mon Jun 30 05:13:09 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello David,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;we had a batch of the LPC1857 which were not configured correctly.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;They start from Flash bank #B instead of #A.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;There is no chance to reverse this setting, you need to replace the chip in case you can't live with that behaviour.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;NXP Support Team&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:21:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1857-Flash-Issues/m-p/537466#M11462</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:21:00Z</dc:date>
    </item>
  </channel>
</rss>