<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Redraw Question - Graph Markers in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Redraw-Question-Graph-Markers/m-p/515311#M1114</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by birdbren on Wed Apr 30 13:42:36 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I’m using EmWin – I’m working with the graph function – I have created objects and a couple of markers that I move back and forth along the graph. The problem I’m having is that the graph appears to redrawing all the objects when I move a marker along the graph and it slows up the functionality the more objects I have on the graph. Is there away (or any sample code) that would allow me just to redraw the marker and not the whole object. I thinking I need to use the validate call but there done not seem to be pone for the graph object – anyway and help on this would be appreciated.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Should the window invalidate / validate be used?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any assistance gudiance would be apprciates.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:17:31 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:17:31Z</dc:date>
    <item>
      <title>Redraw Question - Graph Markers</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Redraw-Question-Graph-Markers/m-p/515311#M1114</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by birdbren on Wed Apr 30 13:42:36 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I’m using EmWin – I’m working with the graph function – I have created objects and a couple of markers that I move back and forth along the graph. The problem I’m having is that the graph appears to redrawing all the objects when I move a marker along the graph and it slows up the functionality the more objects I have on the graph. Is there away (or any sample code) that would allow me just to redraw the marker and not the whole object. I thinking I need to use the validate call but there done not seem to be pone for the graph object – anyway and help on this would be appreciated.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Should the window invalidate / validate be used?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any assistance gudiance would be apprciates.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:17:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Redraw-Question-Graph-Markers/m-p/515311#M1114</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:17:31Z</dc:date>
    </item>
  </channel>
</rss>