<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPCOpen I2C example project slave mode not working: cannot probe or read. in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-I2C-example-project-slave-mode-not-working-cannot-probe/m-p/535486#M11006</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lerlacher on Sun Apr 13 08:41:01 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using the &lt;/SPAN&gt;&lt;A href="http://http://docs.lpcware.com/lpcopen/v1.03/group___e_x_a_m_p_l_e_s___p_e_r_i_p_h__11_x_x___i2_c.html"&gt;LPCOpen I2C example&lt;/A&gt;&lt;SPAN&gt; with an LPC11C24 breakaway board, programmed with LPC-Link.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I just compiled and uploaded the image (with LPC-Link), and it runs, but I can't probe or read the two simulated slave devices.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am doing the probing and reading from a raspberry pi using the linux i2c-tools.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm pretty sure the raspberry pi and the bus are set up correctly. To make sure, I also have an arduino running as a slave on the same bus, and I can probe and read it without problems.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Sadly I don't have a base board here so I don't have a UART connection to use the menu in the example, but the code looks like the slaves should be working despite that.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there anything obvious or any errata in the example code that I'm missing?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Luke&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:38:11 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:38:11Z</dc:date>
    <item>
      <title>LPCOpen I2C example project slave mode not working: cannot probe or read.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-I2C-example-project-slave-mode-not-working-cannot-probe/m-p/535486#M11006</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lerlacher on Sun Apr 13 08:41:01 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using the &lt;/SPAN&gt;&lt;A href="http://http://docs.lpcware.com/lpcopen/v1.03/group___e_x_a_m_p_l_e_s___p_e_r_i_p_h__11_x_x___i2_c.html"&gt;LPCOpen I2C example&lt;/A&gt;&lt;SPAN&gt; with an LPC11C24 breakaway board, programmed with LPC-Link.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I just compiled and uploaded the image (with LPC-Link), and it runs, but I can't probe or read the two simulated slave devices.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am doing the probing and reading from a raspberry pi using the linux i2c-tools.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm pretty sure the raspberry pi and the bus are set up correctly. To make sure, I also have an arduino running as a slave on the same bus, and I can probe and read it without problems.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Sadly I don't have a base board here so I don't have a UART connection to use the menu in the example, but the code looks like the slaves should be working despite that.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there anything obvious or any errata in the example code that I'm missing?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Luke&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:38:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-I2C-example-project-slave-mode-not-working-cannot-probe/m-p/535486#M11006</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:38:11Z</dc:date>
    </item>
  </channel>
</rss>