<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic emWin Application Help in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/emWin-Application-Help/m-p/535033#M10941</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Noufal on Thu Jan 14 09:38:18 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Looking for some help&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1. In my application i want to have a keypad which will have a background image and on top of it individual&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;button with image and on press i need to invoke some function and change the button color(another image with different color), What is the best way to create this application ? Is there any custom keypad example available which uses images as foreground for button and on click change the color of the button?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;2. what is recommended image format( bmp or png or any other format ?) for this application&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;3. what is the correct way to create a keypad? Just use the button&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;and assign image to it or is there a way use images and trigger a call back on press / release on image?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;4. I tried to create the layout using GUIBuilder with bmp as background image, but crashes i add more images, &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;but when i use png i'm able to create this but my application is not working on target with png, So i'm not sure what is the right format to use&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My main concern is having lot of image it could slow down the system, So i want to use the optimum solution which would have faster response&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:20:47 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:20:47Z</dc:date>
    <item>
      <title>emWin Application Help</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/emWin-Application-Help/m-p/535033#M10941</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Noufal on Thu Jan 14 09:38:18 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Looking for some help&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1. In my application i want to have a keypad which will have a background image and on top of it individual&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;button with image and on press i need to invoke some function and change the button color(another image with different color), What is the best way to create this application ? Is there any custom keypad example available which uses images as foreground for button and on click change the color of the button?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;2. what is recommended image format( bmp or png or any other format ?) for this application&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;3. what is the correct way to create a keypad? Just use the button&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;and assign image to it or is there a way use images and trigger a call back on press / release on image?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;4. I tried to create the layout using GUIBuilder with bmp as background image, but crashes i add more images, &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;but when i use png i'm able to create this but my application is not working on target with png, So i'm not sure what is the right format to use&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My main concern is having lot of image it could slow down the system, So i want to use the optimum solution which would have faster response&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:20:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/emWin-Application-Help/m-p/535033#M10941</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:20:47Z</dc:date>
    </item>
  </channel>
</rss>