<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC15xx ADC readings</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC15xx-ADC-readings/m-p/513301#M109</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by kbowers on Thu Aug 28 11:53:07 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The signals are just simple resistor dividers with the lower resistor in the 1k-5k range.&amp;nbsp; I have tried different sampling frequencies from 10kHz up to 100kHz with negligible changes in the readings.&amp;nbsp; I am not using channel 0 to monitor anything externally.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:05:18 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:05:18Z</dc:date>
    <item>
      <title>LPC15xx ADC readings</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC15xx-ADC-readings/m-p/513299#M107</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by kbowers on Thu Aug 28 10:52:42 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am having some issues with the accuracy of the ADC readings on the LPC1549 using the Xpresso V2 board.&amp;nbsp; I am sampling several inputs using burst mode and am seeing relatively accurate readings on ADC1 but not on ADC0 (about 10% high)&amp;nbsp; The driving circuitry on all the channels are almost identical.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have run the calibration cycle on both ADC0 and ADC1 and all the setup configurations are identical.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is it possible that ADC0 is damaged?&amp;nbsp; Can I select channel 0 to be the temperature on both ADC's and compare the values to confirm they are both working correctly?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I was also wondering what the VDDA/2 input to channel 0 should read.&amp;nbsp; Should it not just be 2048 or is there a formula to convert the ADC reading to an actual voltage for VDDA/2.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:05:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC15xx-ADC-readings/m-p/513299#M107</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:05:16Z</dc:date>
    </item>
    <item>
      <title>Re: LPC15xx ADC readings</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC15xx-ADC-readings/m-p/513300#M108</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mc on Thu Aug 28 11:17:30 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi kbowers,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In burst mode the signal source resistance should be low. How are you feeding the signals?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Yes, VDD/2 should read 2048. Please also note that channel 0 is slow channel&amp;nbsp; compared to other channels. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;What is the sampling frequency? &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:05:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC15xx-ADC-readings/m-p/513300#M108</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:05:17Z</dc:date>
    </item>
    <item>
      <title>Re: LPC15xx ADC readings</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC15xx-ADC-readings/m-p/513301#M109</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by kbowers on Thu Aug 28 11:53:07 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The signals are just simple resistor dividers with the lower resistor in the 1k-5k range.&amp;nbsp; I have tried different sampling frequencies from 10kHz up to 100kHz with negligible changes in the readings.&amp;nbsp; I am not using channel 0 to monitor anything externally.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:05:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC15xx-ADC-readings/m-p/513301#M109</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:05:18Z</dc:date>
    </item>
  </channel>
</rss>